Trossen Robotics will be on Holiday Vacation November 26-29. Orders placed after 2:30pm CST on November 25th will be processed on November 30th.
This item is on hold and cannot be ordered at this time - read about product status here
Was: $44.95
Sale: $35.96
You Save: $8.99 (20.0%)
  • Black Friday / Cyber Monday Sale - RobotGeek/Interbotix - 20%
  • Black Friday / Cyber Monday Sale - All Items 10%

This is the 2013 version of the Mech Warfare Half-size Target Panel. Please see the Documentation links below if you are unsure of how many and what type of Target Panels you need. There are also Full-Size Target panels available. You should be familiar with the ruleset and what is required to compete. If you have questions, please post in the Mech Warfare forums (link in Documentation below).
Mounting hole specs & more documentation to come soon!

Please Note: These Half-Size panels can be configured as a single split panel, or as two separate half-size panels.


  • 4x 1.5" Male FSRs
  • 2x ABS Half-size Back Plates
  • 2x Lexan Half-size Front Plates
  • FSR Panel PCB, resistors, Cables

Section VII has information on the number of Target Panels required to compete
FSR Panel Build Tutorial
Mech Warfare Forums (more info here)
Due to high demand and supply chain/production fluctuation, please be aware we cannot guarantee that Interbotix Labs kits will be shipped immediately. We make every possible effort to keep kits in stock, but at times the production lags behind demand for various reasons. For time sensitive projects, please contact for an estimated lead time on our kits and plan purchases with ample time. Orders are shipped in the order they are received as stock allows.