Products 13-24 of 158
Show
Dynamixel MX-12W Front View
Price: $65.90
Availability: In Stock
Item #: RO-902-0086-000 -

    The MX-12W from ROBOTIS is the Goldilocks of servos; everything about it is just right. It has the compact size of the AX-12A and AX-18A (and uses the same housing) yet has the electronics and control capabilities of the high performance MX servos like the MX-28T and MX-64T. This is the only servo at this size and cost, that is capable of true position control for multiple rotations. If you've ever tried to get more than one revolution out of your servo and been frustrated with losing your...

    Dynamixel MX-106T Robot Actuator dynamixel mx-106, dynamixel mx-106T, mx-106, mx-106T, mx-106 robot actuator, mx-106T robot actuator, mx-106 servo, MX-106T servo, MX-106 actuator, dynamixel mx-106 actuator, dynamixel mx-106 robotis, mx-106 robotis, dynamixel
    Price: $493.90
    Availability: In Stock
    Item #: RO-902-0061-000 -

      Dynamixel Comparison Guide The MX-106T Dynamixel Robot Servo Actuator is the newest generation of Robotis Dynamixel actuator; equipped with an onboard 32bit 72mhz Cortex M3, a contact-less magnetic encoder with 4x the resolution over the AX/RX series, and up to 3mpbs using the new TTL 2.0 bus. Each servo has the ability to track its speed, temperature, shaft position, voltage, and load. As if this weren't enough, the newly implemented PID control algorithm used to maintain shaft position can...

      Dynamixel AX-12W Robot Actuator ax-12, ax-12W servo, ax-12W actuator, ax-12W robotis, ax-12W, ax-12+, ax-12A servo, ax-12+ servo, ax-12A actuator, ax-12+ actuator, dynamixel ax-12W, dynamixel ax-12+, dynamixel ax-12
      Price: $44.90
      Availability: In Stock
      Item #: RO-902-0003-000W -

        Dynamixel Comparison Guide The AX-12W servo actuator from Robotis is a wheeled variant of the popular AX-12A. Essentially this servo is an AX-12A with a lower gear ratio so that a much higher RPM can be achieved, making it ideal for use in 'Wheel Mode' as opposed to the traditional 'Joint Mode'. The AX-12W robot servo has the ability to track its temperature, voltage, and load. As if this weren't enough, the control algorithm used to maintain shaft position on the ax-12 actuator can be...

        Dynamixel MX-106R Robot Actuator dynamixel mx-106, dynamixel mx-106R, mx-106, mx-106R, mx-106 robot actuator, mx-106R robot actuator, mx-106 servo, MX-106R servo, MX-106 actuator, dynamixel mx-106 actuator, dynamixel mx-106 robotis, mx-106 robotis, dynamixel
        Price: $499.90
        Availability: In Stock
        Item #: RO-902-0066-000 -

          Dynamixel Comparison Guide The MX-106R Dynamixel Robot Servo Actuator is the newest generation of Robotis Dynamixel actuator; equipped with an onboard 32bit 72mhz Cortex M3, a contact-less magnetic encoder with 4x the resolution over the AX/RX series, and up to 3mpbs using the new RS-485 2.0 bus. Each servo has the ability to track its speed, temperature, shaft position, voltage, and load. As if this weren't enough, the newly implemented PID control algorithm used to maintain shaft position...

          Dynamixel XL-320 Servo Front Photo
          Price: $21.90
          Availability: In Stock
          Item #: RO-902-0087-000 -

            The XL-320 servo from ROBOTIS is so small you might mistake it for an ordinary hobby servo, but you would be missing out! Despite its diminutive size, it is actually one of the newest models in the DYNAMIXEL robot servo line from ROBOTIS. Each XL-320 can produce up to 0.39 N-m (55 in-oz) of torque and rotate at 114 RPM in precisely controlled 0.29° increments. For its size (24 x 36 x 27 mm) and weight (16.7 g) there is no other servo that can compete with the XL-320 in performance and...

            Dynamixel MX-28T Robot Actuator Bulk (6 pack) mx-28, mx-28 actuator, mx-28 robotis, dynamixel mx-28, mx-28 robot, dynamixel mx-28 actuator
            Price: $1,099.50
            Availability: In Stock
            Item #: RO-902-0016-001 -

              Dynamixel Comparison Guide This is a 6 piece Bulk package of the MX-28T. In this bulk pack, the servos are bare and do not come with the required servo horn, nor any additional cables, brackets, or hardware. If you need this hardware, it must be purchased separately. The MX-28T Dynamixel Robot Servo Actuator is the newest generation of Robotis Dynamixel actuator; equipped with an onboard 32bit 72mhz Cortex M3, a contact-less magnetic encoder with 4x the resolution over the AX/RX series, and up...

              Dynamixel MX-28AT Robot Actuator Bulk (6 pack) mx-28, mx-28 actuator, mx-28 robotis, dynamixel mx-28, mx-28 robot, dynamixel mx-28 actuator
              Price: $1,199.50
              Availability: Special Order
              Item #: RO-902-0100-000 -

                Dynamixel Comparison Guide This is a 6 piece Bulk package of the MX-28T. In this bulk pack, the servos are bare and do not come with the required servo horn, nor any additional cables, brackets, or hardware. If you need this hardware, it must be purchased separately. The MX-28AT Dynamixel Robot Servo Actuator is the newest generation of Robotis Dynamixel actuator; equipped with an onboard 32bit 72mhz Cortex M3, a contact-less magnetic encoder with 4x the resolution over the AX/RX series, and...

                Dynamixel MX-28AR Robot Actuator Bulk (6 pack) mx-28, mx-28 actuator, mx-28 robotis, dynamixel mx-28, mx-28 robot, dynamixel mx-28 actuator
                Price: $1,249.50
                Availability: Special Order
                Item #: RO-902-0099-000 -

                  Dynamixel Comparison Guide This is a 6 piece Bulk package of the MX-28R. In this bulk pack, the servos are bare and do not come with the required servo horn, nor any additional cables, brackets, or hardware. If you need this hardware, it must be purchased separately. The MX-28R Dynamixel Robot Servo Actuator is the newest generation of Robotis Dynamixel actuator; equipped with an onboard 32bit 72mhz Cortex M3, a contact-less magnetic encoder with 4x the resolution over the AX/RX series, and up...

                  Dynamixel MX-64T Robot Actuator Bulk (6 pack) dynamixel mx-64 robot actuator robotis, mx64, dynamixel mx-64 robot actuator, dynamixel mx-64 actuator, dynamixel mx-64 robotis, dynamixel mx-64, dynamixel, mx-64 robot actuator robotis, mx-64 robot actuator, mx-64 actuator, mx-64 robotis, mx-64
                  Price: $1,499.50
                  Availability: On Hold
                  Item #: RO-902-0069-000 -

                    Dynamixel Comparison Guide This is a 6 piece Bulk package of the MX-64T. In this bulk pack, the servos are bare and do not come with the required servo horn, nor any additional cables, brackets, or hardware. If you need this hardware, it must be purchased separately. The MX-64T Dynamixel Robot Servo Actuator is the newest generation of Robotis Dynamixel actuator; equipped with an onboard 32bit 72mhz Cortex M3, a contact-less magnetic encoder with 4x the resolution over the AX/RX series, and up...

                    Dynamixel MX-64AT Robot Actuator Bulk (6 pack) dynamixel mx-64 robot actuator robotis, mx64, dynamixel mx-64 robot actuator, dynamixel mx-64 actuator, dynamixel mx-64 robotis, dynamixel mx-64, dynamixel, mx-64 robot actuator robotis, mx-64 robot actuator, mx-64 actuator, mx-64 robotis, mx-64
                    Price: $1,549.50
                    Availability: Special Order
                    Item #: RO-902-0102-000 -

                      Dynamixel Comparison Guide This is a 6 piece Bulk package of the MX-64T. In this bulk pack, the servos are bare and do not come with the required servo horn, nor any additional cables, brackets, or hardware. If you need this hardware, it must be purchased separately. The MX-64AT Dynamixel Robot Servo Actuator is the newest generation of Robotis Dynamixel actuator; equipped with an onboard 32bit 72mhz Cortex M3, a contact-less magnetic encoder with 4x the resolution over the AX/RX series, and...

                      Dynamixel Pro L42-10-S300-R Robot Actuator
                      Price: $590.00
                      Availability: Special Order
                      Item #: RO-902-0092-000 -

                        The DYNAMIXEL PRO line of Robot Actuators is ROBOTIS's new solution for full-scale robots. These new actuators have incredibly high power and precision, making them ideal for for everything from advanced robotics to industry applications. Using ROBOTIS's frame system for the DYNAMIXEL PRO, you'll be able to rapidly create a variety of different systems and robots. These new servos have position, speed, AND torque based commands. The L42-10-S300-R uses a RS-485 communication protocol, a 300:1...

                        Dynamixel MX-64AR Robot Actuator Bulk (6 pack) dynamixel mx-64 robot actuator robotis, mx64, dynamixel mx-64 robot actuator, dynamixel mx-64, dynamixel mx-64 robotis, dynamixel mx-64, dynamixel, mx-64 robot actuator robotis, mx-64 robot actuator, mx-64 actuator, mx-64 robotis, mx-64
                        Price: $1,599.50
                        Availability: Special Order
                        Item #: RO-902-0101-000 -

                          Dynamixel Comparison Guide This is a 6 piece Bulk package of the MX-64AR. In this bulk pack, the servos are bare and do not come with the required servo horn, nor any additional cables, brackets, or hardware. If you need this hardware, it must be purchased separately. The MX-64AR Dynamixel Robot Servo Actuator is the newest generation of Robotis Dynamixel actuator; equipped with an onboard 32bit 72mhz Cortex M3, a contact-less magnetic encoder with 4x the resolution over the AX/RX series, and...