Products 37-48 of 78
Show
Grove - Buzzer Grove Buzzer, Arduino buzzer, buzzer, arduino sound
Price: $4.95
Availability: In Stock
Item #: SS-COM22458P -

    Description This is a simple yet enjoyable Grove to use. The piezo can be connected to digital outputs, and will emit a tone when the output is high. Alternatively it can be connected to an analog pulse-width modulation output to generate various tones and effects. Documents Please visit our wiki page for more info about this product. ...

    Grove - Touch Sensor Grove Touch Sensor, Arduino touch sensor, touch sensor, grove touch sensor
    Price: $4.95
    Availability: Back Order
    Item #: SS-SEN11303P -

      Description This is a simple touch sensor module. You can use it to replace a traditional push button. Using the TTP223-B touch detector IC It measures the capacitance of a metallic pad. It can detect the change in capacitance when a finger is near it. This is the same technology used in the iPhone touch screen. So you can place the metallic pad under a non-metallic surface such as a plastic or glass sheet and it will still work as a button. This may be useful for projects that need to be...

      Grove - Rotary Angle Sensor Grove Rotary Angle Sensor, Rotary Angle Sensor, arduino potentiometer, turn knob
      Price: $4.95
      Availability: In Stock
      Item #: SS-COM22735P -

        Description The potentiometer Grove produces analog output between 0 and Vcc (5V DC with Seeeduino) on its D1 connector. The D2 connector is not used. The angular range is 300 degrees with a linear change in value. The resistance value is 10k ohms, perfect for Arduino use. This may also be known as a rotary angle sensor. Document How to use ...

        Grove - Light Sensor Grove Light Sensor, arduino light sensor, freeduino light sensor, seeeduino light sensor
        Price: $4.95
        Availability: Back Order
        Item #: SS-SEN11302P -

          Description The Light sensor module uses the GL5528 photoresistor to detect the light intensity of the environment. The resistance of the sensor decreases when the light intensity of the environment increases. The chip LM358 is used as a voltage follower to enable you get a accurate data. Features Grove compatible interface Wide supply voltage range: 3V-30V 2.0cm x 2.0cm Grove module? Minimum external parts Applications Ideas Electronic toys Light-control switch Monitor Documents Please visit...

          Grove - Electricity Sensor Grove Electricity Sensor, arduino electricity sensor, electrical sensor, electricity detection sensor
          Price: $7.95
          Availability: In Stock
          Item #: SS-SEN23931P -

            Description The Electricity sensor module is a member of Grove. It is based on the TA12-200 current transformer which can change large alternating current into a small amplitude. You can use it to test large alternating current upto 5A. Features Grove compatible interface Maximum 5A input High accuracy Small size Applications Alternating current measurment Device condition monitoring Document Datasheet ...

            Grove - Serial LCD 16x2 Grove Serial LCD, Grove Serial LCD 16x2, Serial LCD, Seeedstudio LCD, Arduino LCD, Arduino Display, Grove LCD
            Price: $14.95
            Availability: In Stock
            Item #: SS-LCD23154P -

              Description Serial LCD Driver Grove is an UART based LCD1602 display (Hitachi HD44780 or a compatible LCD). It can control LCD1602 only with two I/O port pins (UART Tx and Rx).The VCC and GND are the only additional pins required for operation. Conventional LCD drivers use 7-11 I/O port pins, whereas Serial LCD grove saves all these additional I/O pins. Serial LCD grove uses AT89S52 for implementing the UART Driving logic. Now has been updated to v1.0b. Features Very easy to use. 4-Pin...

              Grove - Temperature Sensor Grove Temperature Sensor, Grove sensor, Temperature Sensor, arduino temperature sensor, freeduino sensor, seeeduino sensor
              Price: $4.95
              Availability: In Stock
              Item #: SS-SEN23292P -

                Description The temperature sensor Grove uses a thermistor which returns the ambient temperature in the form of a resistance value, which is then used to alter Vcc (5V with our Seeeduinos). Our board then converts this voltage value measured by an analog input pin to a temperature. The operating range is -40 to 125 degrees Celsius, with an accuracy of ?1.5?C. Document Datasheet How to use ...

                Grove - Temperature & Humidity Sensor Grove Temperature Sensor, Grove Humidity Sensor, Grove Temperature Humidity Sensor Grove sensor, Temperature Humidity Sensor, arduino temperature sensor, freeduino sensor, seeeduino sensor
                Price: $6.95
                Availability: Back Order
                Item #: SS-SEN11301P -

                  Description This temperature & humidity sensor provides a pre-calibrated digital output. A unique capacitive sensor element measures relative humidity and the temperature is measured by a negative temperature coefficient (NTC) thermistor. It has excellent reliability and long term stability. Please note that this sensor will not work for temperatures below 0 degree. Features Relative Humidity and temperature measurement Full range temperature compensation Calibrated Digital signal Long...

                  Grove- 5V Relay Module
                  Price: $6.95
                  Availability: In Stock
                  Item #: SS-COM22639P -

                    Description The Relay Grove is a digital normally open switch that controls a relay capable of switching much higher voltages and currents than your normal Arduino boards. When set to HIGH, the LED will light up and the relay will close allowing current to flow. The peak voltage capability is 250V at 10 amps. Please exercise great care when working with mains voltages— if in doubt contact a professional such as a licensed electrician for help. Document How to use ...

                    Adjustable Breadboard Power Supply Adjustable, Breadboard, Power Supply, arduino, freeduino
                    Price: $15.37
                    Availability: In Stock
                    Item #: SS-TOL123D3P -

                      Another breadboard power supply designed by Seeed Studio. it can directly takes power from DC wall wart and outputs a selectable 5V or 3.3V regulated voltage. Compared to other breadboard power supply designs; this one provides mini-USB port like the seeeduino, you can toggle the switch and select your power source. (USB or dc jack). We also used JST-2pin power jack, the one as on Seeeduino. With this board, you can send power to both power lane of the breadboard, and each side has a on/off...

                      Foot Switch Foot, Switch, pedal, physical, input, computing, arduino, freeduino, seeeduino
                      Price: $5.50
                      Availability: Back Order
                      Item #: SS-SWT129C6B -

                        Building an electronic music project? Need to step on the gas? Perhaps this is the final component for your sub-orbital space fighter? Whatever your application is, this Foot Switch is perfect for all applications in need of a Foot Switch!

                        Grove - PIR Motion Sensor Grove - PIR Motion Sensor
                        Price: $9.95
                        Availability: Back Order
                        Item #: SS-SEN32357P -

                          This is a simple to use PIR motion sensor with Grove compatible interface. When anyone moves within the detection range the sensor outputs HIGH on its SIG pin. The detection range and response speed can be adjusted by the two on-board potentiometers. The response time can be adjusted from 0.3s to 25s with up to 6 meters of detecting range! Product WIKI Page. Specifications Grove compatible interface Adjustable detection distance and response time Voltage range: 3V–5V 2.0cm x 4.0cm Detecting...