Home > Robot Parts > I/O Boards & Robot Controllers > Atmel & Arduino >
Orangutan USB AVR Programmer
Item #:
C-400-740
Availability: In Stock
Price: $27.95
Quantity Count | Price Each |
| 20 | $24.95 |
| 51 | $22.95 |
| 101 | $20.95 |
| This compact programmer can program the a variety of Atmel AVR based robot controllers, as well as the 3pi robot, through a USB connection. The on-board USB-to-serial adapter allows the unit to look like a serial AVRISP programmer to your programming software. The serial port TX and RX lines are connected to separate pads so that the programmer can also be used as a USB-to-serial adapter. |
| |
A USB A to Mini-B cable is required but not included. These types of cables are common for digital cameras and other USB peripherals, so you might already have the necessary cable. The 6-pin ISP programming cable is included. The older, 10-pin ISP connections are not directly supported.
Using the USB programmer
Begin by following the USB-to-serial adapter driver installation instructions. Make sure you install the driver before you connect your programmer to the computer. The USB adapter will install as two devices (USB device and COM port); you can ignore Microsoft’s repeated warnings that the driver has not been tested by Microsoft. Once the driver is installed, your programming software can communicate with the programmer as if it were on a serial port.
The programmer is powered through the USB port, but it does not deliver that power to the target device. Your target device must therefore be turned on to be programmed. Be careful about the pin 1 orientation with the Baby Orangutan, which does not have a shrouded ISP connector. The red wire and mark on the ISP connector should be lined up with the arrow to pin 1 on the Baby Orangutan PCB. The Orangutan, Orangutan SV-xx8, Orangutan LV-168, and 3pi robot all have keyed shrouded headers that enforce proper orientation of the ISP cable.
The USB-to-serial adapter functionality can be accessed through the pads on the side of the PCB labeled TX, RX and G (for ground). The TX line (from the computer’s perspective—connect it to your target device’s RX line) is always connected, but the RX line needs to be switched using the shorting block in the middle of the board. Connecting it on the “P” side allows for programmer operation; the “U” side allows user USB adapter operation.
Please see our Orangutan USB Programmer User’s Guide for more detailed information, usage instructions, and troubleshooting help.
|