The
pcProx USB RFID Reader has little brother, the
pcProx USB Dongle Reader! This diminutive reader is compatible with all
EM4102 (125 kHz)RFID tags. Out of the box, this reader will read RFID tags and translate them into keystrokes, just as if they had been typed by a computer. The powerful yet intuitive configuration software can be used to configure the reader’s output with various formatting options.In most common uses, the reader emulates a keyboard and keystrokes the card’s ID and/or site code to the cursor’s location on the screen. The reader can be configured to add keystrokes before or after the card’s data to faciliate different functions and compatiblity.
Using the pcProx reader, you can create a variety of secure log-on scenarios. You can use single-factor authentication, where the RFID card provides the entire password, or deply two-factor authetication, where the RFID card is paired with a second authetication form like PIN number, password, etc.