- 1.5 mm Hex Driver (Included)
- 2.5 mm Hex Driver (Included)
- Needle-Nose Pliers
- Small Flat Head Screw Driver
|
 |
|
Note: Some of the parts in some assemblies come packaged in separate smaller bags because they come with a bracket or other various part. Please review the entire parts list to ensure you have all necessary components. Some kits will have spare bolts, nuts, or screws included.
|
 |
| 1 X |
1 X |
1 X |
 |
|
 |
|
 |
 |
 |
| 1 X |
1 X |
1 X |
 |
|
|
|
 |
 |
 |
| 1 X |
1 X |
2 X |
 |
|
|
|
 |
 |
 |
| 1 X |
1 X |
1 X |
 |
|
|
|
 |
 |
 |
| 1 X |
1 X |
1 X |
 |
|
|
|
 |
 |
 |
| 1 X |
1 X |
1 X |
 |
|
|
 |
 |
 |
 |
| 1 X |
7 X |
1 X |
 |
 |
 |
 |
 |
 |
 |
| 1 X |
3 X |
2 X |
 |
|
|
 |
 |
 |
 |
| 2 X |
1 X |
1 X |
 |
 |
|
 |
 |
 |
 |
| 1 X |
|
|
 |
 |
|
|
 |
 |
| 20 X |
86 X |
46 X |
16 X |
 |
|
|
|
 |
 |
 |
 |
 |
 |
| 4 X |
5 X |
9 X |
33 X |
 |
|
|
|
 |
 |
 |
 |
 |
 |
 |
|
|
|
| 6 X |
6 X |
12 X |
150 X |
 |
|
|
|
 |
 |
 |
 |
 |
 |
 |
|
|
|
| 6 X |
21 X |
9 X |
5 X |
 |
|
|
|
 |
 |
 |
 |
 |
 |
 |
|
|
|
| 5 X |
5 X |
1 X |
2 X |
 |
|
|
|
 |
 |
 |
 |
 |
 |
 |
|
|
|
| 27 X |
2 X |
8 X |
1 X |
 |
|
|
|
 |
 |
 |
 |
 |
|
|
|
| ASSEMBLY TIPS: Seating the Nuts into the Nut Sockets |
| |
|
| ASSEMBLY TIPS: Assemble in the Correct Order |
Make note of the servo IDs and their positions. Each servo has a # written on the back of it. Be sure you assemble the servos in the correct order so that your arm will work!
| ASSEMBLY TIPS: Check Horn Orieintation |
Each AX-12A servo should ship with the horn alined to 'Center'. The horn is correctly centered when the single notch on the horn matches the single notch on the servo body. As you put together your arm, make sure that the servos are centered as you attach the brackets in the pictures. Incorrect servo orientation will cause problems with your robot.
|
| |
|
First prep (2) F2 Brackets and (2) F4 Brackets with M2 Nuts as shown.
| 32x |
|
 |
|
|
|
|
|
| |
|
Mount an F2 Bracket to Servos #2 and #3 each.
| 2x |
2x |
 |
 |
|
| 8x |
|
 |
|
|
|
|
|
| |
|
Mount the F4 Brackets to Servos #4 and #5.
*Note the orientation of the brackets as shown.
| 2x |
2x |
 |
 |
|
| 8x |
|
 |
|
|
|
|
|
| |
|
Assemble the runners of each side by mounting the Inside Arm Covers and Outside Arm Covers connecting Servos #2 to #4, #3 to #5.
*Note servos will need to be prepped with M2 Nuts in respective positions for mounting.
| 60x |
60x |
 |
 |
|
|
|
|
| |
|
Take time to run the cables for the servos as shown.
| 3x |
2x |
 |
 |
|
|
|
|
| |
|
Mount a 30mm F-F Standoff with (3) Spacers to the Bottom Arm Cover.
|
|
|
| |
|
Complete for all mounting holes (6x) on Bottom Arm Cover.
| 6x |
18x |
 |
 |
|
| 6x |
|
 |
|
|
|
|
|
| |
|
Assemble the Bottom Arm Cover slots along with the Top Arm Cover slots onto the runner tabs as shown and mount.
| 6x |
|
 |
|
|
|
|
|
| |
| |
|
Sit the Locking Plate tabs into the slots of the Bottom Forearm Bracket and make sure to run the cable from the Middle Arm Section through the hole and slot up to Servo #6. |
|
| |
|
Mount (5) sets of 10mm F-F and 15mm M-F standoffs to the Forearm Cover Bracket.
*Note the orientation of the standoffs in picture.
| 5x |
5x |
 |
 |
|
| 5x |
|
 |
|
|
|
|
| |
|
Insert the tabs of the Locking Plates along with the (2) Side Forearm Plates and Forearm Bottom Bracket into the slots of the Forearm Cover from the back. |
|
| |
|
Attach the second Forearm Cover from the front as shown.
| 5x |
|
 |
|
|
|
|
 |
|
|
| |
|
Prep your F2 Bracket with M2 Nuts as shown.
| 4x |
|
 |
|
|
|
|
|
|
|
|
|
|
For increased wrist range, an F1 Bracket has been included in the kit that can be substituted in for the F2 Bracket in the step above.
For even more range, using a pair of flat and angled nippers, the inside edge of the F1 can be removed. |
|
|
 |
|
Mount the bottom TWO holes only, of the Bottom Back Bracket to the F2 Bracket.
| 2x |
|
 |
|
|
|
|
 |
|
|
If you chose TO ADD the Wrist Rotation Servo in your Arm Assembly, follow the link to continue your assembly.
Wrist Rotation Servo Assembly
If not, proceed with the Assmbley Guide below and ignore Servo #7.
|
|
|
Next mount the Top and Bottom Back Brackets to the back of Servo #8.
*Note servos will need to be prepped with M2 Nuts in respective positions for mounting.
| 6x |
6x |
 |
 |
|
|
|
|
 |
| |
|
Finish mounting the top (2) holes of the Bottom Back Bracket to the F2 Bracket.
| 2x |
|
 |
|
|
|
|
 |
|
|
 |
| |
|
Mount the F2 Bracket to Servo #6 of the Upper Arm Section.
| 1x |
1x |
 |
 |
|
| 4x |
|
 |
|
|
|
|
 |
| |
|
Put in the final cable through the slot in the F2 Bracket from Servos #6 to #8.
| 1x |
|
 |
|
|
|
|
 |
| |
|
Connect your Pigtails to the ArbotiX.
*Note the polarity of the the ArbotiX when connecting. |
|
 |
| |
|
Connect your FTDI Cable to the Arbotix.
*Note the polarity of the the ArbotiX when connecting.
|
|
 |
| |
|
Lastly, feed the wires out the back and above the Bottom Base and use Zip Ties to secure the wires as shown.
| 2x |
|
 |
|
|
|
|
 |