| STEP 10 - Setting up the power supply |
| |
|
(It should be fairly obvious to NOT have the power supplies plugged in during the following steps. If you haven't figured that out please send the robot back to us and find a new hobby/career.)
|
| |
|
Your Robot Turret comes with two power supplies. The 12 volt power supply is for the logic, the arbotiX board, and the 16 volt variable power supply is for the servo power which attaches to the rX Bridge.
|
 |
 |
Clip the ends off the two power supplies.
(Why doesn't the arbotiX have power jacks? The arbotiX is traditionally a mobile robot controller powered by batteries and that is why it has terminal blocks.)
|
|
 |
 |
Strip and twist the wires as shown leaving about 1.5 cm of bare wire.
For the 12V power supply:
Red = Positive (+)
Black = Negative (-)
For the variable power supply:
Brown = Positive (+)
Blue = Negative (-)
|
|
 |
 |
Fold the bare wires in half and twist some more. This makes them thicker and helps provide a much more secure fit in the terminal blocks.
|
|
 |
 |
Remove the J1 jumper from the arbotiX
|
|
 |
 |
Mount the rX bridge as shown using the Hex Button Head 4-40 x 3/4" bolt and the plastic spacer.
| 1 x |
1 x |
 |
 |
|
|
 |
 |
Screw the power supply wires into the terminal blocks.
Make sure the 12 Volt power supply is on the lower terminal block on the main board and the 16 volt variable power supply is on the rX bridge.
MAKE SURE YOUR POLARITIES ARE CORRECT.
On the main board make sure the POSITIVE RED WIRE IS IN THE RIGHT SIDE OF THE TERMINAL BLOCK.
On the rX bridge make sure the POSITIVE BROWN WIRE IS IN THE LEFT TERMINAL BLOCK.
|
|
 |
 |
Set the Variable power supply to 18 volts. The switch should be 2 clicks to the right. The printed voltages and lines are sometimes lined up poorly. Make sure to count the clicks instead of relying on the white lines.
|
|
| STEP 12 - Mount the top section to the Bottom Base Plate |
| |
 |
 |
Use a servo cable to plug the Tilt Servo into the Pan Servo as shown. (You can use which ever jacks you prefer. The order does not matter.)
|
|
 |
 |
Plug in the second Servo Cable to the free Pan Servo Jack. Route the Servo Cable through a slot on the upper base. (Again, jack preference is up to customer.)
|
|
 |
 |
Screw the M/F 6-32 5/8" standoff into the F/F 6-32 1.25" standoff. Tighten them snugly by rotating about a quarter turn past when the faces touch.
| 4 x |
4 x |
 |
 |
|
|
 |
 |
Mount the standoffs to the upper base using four 6-32 x 1/2" hex button head bolts.
| 4 x |
|
 |
|
|
|
 |
 |
Mount the top base to the bottom base as shown using four Hex Button Head 6-32 1/2" bolts. The best orientation is to have the blue terminal power blocks on the back side facing the same way as the back lip of the F8 Frame.
| 4 x |
|
 |
|
|
|
 |
 |
Plug the servo cable into the rX Bridge.
|
|
 |
 |
Plug the FTDI into the arbotiX. Make sure you have the black wire on the right.
|
|