you will need to activate java to view this menu by Deluxe-Menu.com
The goal of our contests have always been to inspire technological creativity, innovation and ingenuity through these talented individual’s unique projects. We invite everyone to help spread the word about this contest announcement to help encourage others to show off their talent.
Retail: $1,299.00
InterbotiX PhantomX Hexapod
Retail: $399.00
Headplay VR Goggles
Retail: $150.00
Roboni-I
Questions? Contact Us!
It is pretty much a known fact at this point that Interlink FSRs totally rock. For low cost yet durable pressure & force sensing they are a great solution. The brilliant minds over at Interlink even made them standard with thin rubber backing that has an adhesive layer. The only complaint some have is that the sensors only came with thin male tabs which can be a pain to solder. Especially if you were working on a project that required dozens or more sensors. The male tabs are still available and are still a great solution for those that need a low profile sensor, but for those that don’t have a thickness constraint female connectors are now here.
Female connectors make it very easy to connect and disconnect the FSRs now. Each female connector FSR comes with a coupling pin so that it can be plugged directly into 1 pin & 2 pin jumper wires or a breadboard. The female connector is standard .1″ spacing so it can also plug right into board headers if needed. No more soldering hassles.
The Robot Turrets hath cometh! We’re proud to announce the first robot kits from InterbotiX Labs, a comprehensive line of high-end pan/tilt turrets. These high speed, high strength, and high performance robot turrets are built from your choice of Robotis Dynamixel Servos, the ArbotiX Robocontroller, and custom lasercut ABS frame components. Just how high speed and high strength are they might you ask? Funny you should mention that! We have prepared these demonstration videos to showcase exactly that. While they lack any true empirical data, repeatability, verifiable results, control groups, or any resemblance to true scientific testing… they are definitely more fun to watch and also contain stuffed monkey abuse, so check em out! For those of you serious about your panning and your tilting!
SPEED!
STRENGTH!
Also: PAINTBALLS!
Robot Pioneers is a short documentary about people who are passionate about robotics. We’ve had the privilege of meeting a plethora of fantastic innovators over the years; through our own online community, at Robogames, via various business communications, universities, techshops, hackerspaces, and at a number of tradeshows.
Each of these makers has a story to tell, and with this short documentary we hope to showcase even just a glimpse of the inspiration we draw from connecting with our fellow grassroots engineers. The future of technology is often grown in one’s own backyard and is open for anyone with the will and want to get involved. Build. Create. Innovate. Make. Join the Robot Revolution!
Sourcing the right eyeballs for your bot can be a pain. With the help of our awesome community of roboticists we have identified some great cameras for each level of price point and quality from low cost to high end research.
We have the cameras in stock now. Stay tuned because soon we will offer them with custom made brackets for mounting solutions making your life just that much easier!
Need something cheap and small?
Grab the Microsoft LifeCam VX-800 Webcam for a mere $19.95
Quality Webcam more your pace?
The Microsoft LifeCam Cinema Webcam – 720p HD is an AMAZING BUY giving you HD for $59.99
Need to go wireless for teleprescence or offloading processing? The perfect video solution for your next Mech Warfare entry?
We got you covered with TRENDnet TV-IP110W WiFi Camera for $119.95
and coming soon, the Firefly research camera from Point Grey.
PhidgetSpatial 0/0/3 is a 3 axis Accelerometer which measures static and dynamic acceleration in 3 axes, up to 5g, and provides a high sampling speed of up to 1000 samples per second.
PhidgetSpatial 3/3/3, 9 Axis IMU (Inertial Measurement Unit) measures static and dynamic acceleration in 3 axes, up to 5g.; it also measures magnetic field in 3-axes up to ±4 Gauss and finally measures angular rotation in 3 axes, up to ±400° per second.
You have to use the right tool for the job Beavis. We now have American made JIS Philips head screwdrivers and Hex keys which are extremely tough and won’t strip or wear. Great news for those of you who have had to deal with the annoyance of cheap imports that barely make it through a single build. We also now stock Turbo Lock for a great low price of $9.95 per 10ml. Be a manly geek and git yourself sum new tools!