Arm Puppeteering

Attention

This documentation site has been moved. Please refer to its new location in the future.

View Package on GitHub

Overview

Imagine that you have two (or more) Interbotix arms with the same number of joints. What the xsarm_puppet allows you to do is to manually manipulate one of the arms and watch as the motion is repeated in real time on the second robot. A potential application of this could be a warehousing environment. Instead of a worker straining his back to lift a heavy package, he could manually manipulate a small version of a robotic arm to maneuver an industrial-sized arm to pick it up.

Structure

../_images/xsarm_puppet_flowchart.png

The above diagram shows the structure for the ‘puppet control’ feature. The nodes involved are:

  • xsarm_puppet - responsible for reading the current joint states from one arm and then publishing them as position commands to a second arm; it accepts two robot names as parameters - robot_name_master and robot_name_puppet
  • static_transform_publisher - two of these nodes are launched to specify the position of both arms relative to the RViz ‘world’ frame
  • rviz - only launch one instance of RViz with two RobotModels for the two robot arms

Usage

To run this feature, plug two robots with the same number of joints (ex. the PincherX-150 and WidowX-250) into two USB ports and in a terminal, type:

$ roslaunch interbotix_xsarm_puppet xsarm_puppet.launch robot_model_master:=px150 robot_model_puppet:=wx250

It might be good idea to verify which robot is given ttyUSB0 as its port name so that you know which robot should be manually manipulated. Do this by only plugging one robot into your computer and looking at the name in the /dev directory before plugging in the second one. Next, manually manipulate the first arm and observe how the second arm closely mimics the motion! To see other command line arguments for the ‘xsarm_puppet.launch’ file, refer to the table below.

Argument Description Default Value
robot_model_master model type of the master Interbotix Arm (the one being physically manipulated) “”
robot_model_puppet model type of the puppet Interbotix Arm (the one that is torqued on and that responds to commands) “”
base_link_master name of the ‘root’ link on the ‘master’ arm; typically ‘base_link’, but can be changed if attaching the arm to a mobile base that already has a ‘base_link’ frame ‘base_link’
base_link_puppet name of the ‘root’ link on the ‘puppet’ arm; typically ‘base_link’, but can be changed if attaching the arm to a mobile base that already has a ‘base_link’ frame ‘base_link’
master_modes the file path to the master ‘mode config’ YAML file refer to xsarm_puppet.launch
puppet_modes the file path to the puppet ‘mode config’ YAML file refer to xsarm_puppet.launch
use_puppet_rviz launches RViz to show both arms true
rvizconfig file path to the config file RViz should load refer to xsarm_puppet.launch
launch_driver true if the xsarm_control.launch file should be launched - set to false if you would like to run your own version of this file separately true
use_sim if true, the Dynamixel simulator node is run; use RViz to visualize the robot’s motion; if false, the real Dynamixel driver node is run false

Video Tutorials

Puppet Control X-Series Arm Demo


Working With Multiple Arms