Gazebo Configuration

Attention

This documentation site has been moved. Please refer to its new location in the future.

View Package on GitHub

Overview

This package contains the necessary config files to get any of the many Interbotix X-Series arms simulated in Gazebo. Specifically, it contains the interbotix_texture.gazebo file which allows the black texture of the robotic arms to display properly (following the method explained here). It also contains YAML files with tuned PID gains for the arm and gripper joints so that ros_control can control the arms effectively. This package has one of two applications. It can either be used in conjunction with MoveIt via the FollowJointTrajectory interface or it can be used by itself via the JointPositionController interface.

Structure

../_images/xsarm_gazebo_flowchart.png

As shown above, the interbotix_xsarm_gazebo package builds on top of the interbotix_xsarm_descriptions and gazebo_ros packages. To get familiar with the nodes in the interbotix_xsarm_descriptions package, please look at its README. The other nodes are described below:

  • gzserver - responsible for running the physics update-loop and sensor data generation
  • gzclient - provides a nice GUI to visualize the robot simulation
  • controller_manager - responsible for loading and starting a set of controllers at once, as well as automatically stopping and unloading those same controllers
  • spawn_model - adds the robot model as defined in the ‘robot_description’ parameter into the Gazebo world

Usage

To run this package, type the line below in a terminal (assuming the WidowX-250 is being launched with trajectory controllers). Note that if you’re using a 4 or 6 dof arm, you should set the dof launch file argument appropriately.

$ roslaunch interbotix_xsarm_gazebo xsarm_gazebo.launch robot_model:=wx250 use_trajectory_controllers:=true

Since by default, Gazebo is started in a ‘paused’ state (this is done to give time for the controllers to kick in), unpause the physics once it is fully loaded by typing:

$ rosservice call /gazebo/unpause_physics

This is the bare minimum needed to get up and running. Take a look at the table below to see how to further customize with other launch file arguments.

Argument Description Default Value
robot_model model type of the Interbotix Arm such as ‘wx200’ or ‘rx150’ “”
robot_name name of the robot (typically equal to robot_model, but could be anything) $(arg robot_model)
base_link_frame name of the ‘root’ link on the arm; typically ‘base_link’, but can be changed if attaching the arm to a mobile base that already has a ‘base_link’ frame base_link’
show_ar_tag if true, the AR tag mount is included in the ‘robot_description’ parameter; if false, it is left out; set to true if using the AR tag mount in your project false
show_gripper_bar if true, the gripper_bar link is included in the ‘robot_description’ parameter; if false, the gripper_bar and finger links are not loaded to the parameter server. Set to false if you have a custom gripper attachment true
show_gripper_fingers if true, the gripper fingers are included in the ‘robot_description’ parameter; if false, the gripper finger links are not loaded to the parameter server. Set to false if you have custom gripper fingers true
use_world_frame set this to true if you would like to load a ‘world’ frame to the ‘robot_description’ parameter which is located exactly at the ‘base_link’ frame of the robot; if using multiple robots or if you would like to attach the ‘base_link’ frame of the robot to a different frame, set this to false true
external_urdf_loc the file path to the custom urdf.xacro file that you would like to include in the Interbotix robot’s urdf.xacro file “”
use_rviz launches RViz true
world_name the file path to the Gazebo ‘world’ file to load refer to xsarm_gazebo.launch
gui launch the Gazebo GUI true
debug Start gzserver in debug mode using gdb false
paused start Gazebo in a paused state true
recording enable Gazebo state log recording false
use_sim_time tells ROS nodes asking for time to get the Gazebo-published simulation time, published over the ROS topic /clock true
use_position_controllers set to true to have the ability to command arbitrary positions to the arm joints in Gazebo false
use_trajectory_controllers set to true to have the ability to command joint trajectories to the arm joints in Gazebo false
dof degrees of freedom of the specified arm (only necessary if use_position_controllers is set to true) 5

Video Tutorial

Working with the Interbotix Arm in Gazebo