PID Gains Test Environment
Attention
This documentation site has been moved. Please refer to its new location in the future.

Overview
This package can be used as a way to test ‘pwm’ or ‘current’ PID gains when operating the arm in either ‘pwm’ or ‘current’ mode. PID gains are read into the controller node from the gains.yaml file. The node then commands the arm to its ‘home’ pose and waits ten seconds for it to settle. Then it commands the arm to its ‘sleep’ pose and waits another ten seconds for it to settle. Finally, the node commands all the motors to either zero pwm or zero current (effectively torquing them off) before shutting itself down.
Structure

As shown above, the interbotix_xsarm_pid package builds on top of the interbotix_xsarm_control package. To get pointers about the nodes in the that package, please look at its README. The node specific to this package is described below.
- xsarm_pid - contains a simple PID controller to command the arm joints (excluding gripper)
first to their ‘home’ positions and then to their ‘sleep’ positions; it receives the desired
PID gains from gains.yaml and the
control_mode
as a parameter.
Usage
To run this package, first create a ‘gains.yaml’ file similar to the one here with your desired ‘pwm’ or ‘current’ PID gains. Then run the command below (assuming the ReactorX-150 is being used in ‘pwm’ mode).
$ roslaunch interbotix_xsarm_pid xsarm_pid.launch robot_model:=rx150 control_mode:=pwm
To further customize the launch of the robot, take a look at the table below.
Argument | Description | Default Value |
---|---|---|
robot_model | model type of the Interbotix Arm such as ‘wx200’ or ‘rx150’ | “” |
robot_name | name of the robot (typically equal to robot_model, but could be anything) | $(arg robot_model) |
base_link_frame | name of the ‘root’ link on the arm; typically ‘base_link’, but can be changed if attaching the arm to a mobile base that already has a ‘base_link’ frame | base_link’ |
use_rviz | launches RViz | true |
mode_configs | the file path to the ‘mode config’ YAML file | refer to xsarm_pid.launch |
control_mode | the outputted command from the control loop - can be either ‘pwm’ or ‘current’ | pwm |
gains_filepath | the file path to the ‘gains’ YAML file | refer to xsarm_pid.launch |
launch_driver | true if the xsarm_control.launch file should be launched - set to false if you would like to run your own version of this file separately | true |