top of page

DIY UMI vs TRumi vs PiKA: Choosing a Handheld Robot Data Collection System

Jul 10
4 min read

The Short Version

  • Pick DIY Stanford UMI when you need open-source control and have build, SLAM, and maintenance capacity.

  • Choose TRumi from Trossen Robotics when you're past 'can we build one?' and need reliable, scalable collection.

  • Consider AgileX PiKA when your workflow depends on its multimodal sensor stack, base station, and matched components.

  • Output structured datasets by exporting Zarr or MCAP through Trossen Data Collection Pipelines.

  • Standardize devices and operator workflow when your team needs to scale bimanual or multi-site collection.

  • Pair TRumi with leader-follower teleoperation when robot-specific tuning and validation are still needed.

  • Start from the UMI GitHub repo if you're reproducing the Stanford paper or modifying hardware.


Who this is for

  • Robotics labs with build capacity

  • Startups and data teams

  • Enterprise R&D groups

  • Embodied AI researchers

  • Teams evaluating handheld data collection systems


DIY UMI is best for research teams that want maximum control and can build, debug, and maintain the system. TRumi is best for teams that want a supported UMI-style handheld manipulation data collection system with structured Zarr or MCAP outputs. PiKA is a higher-integration commercial system with its own sensor and positioning approach.


TRumi is Trossen Robotics’ engineered and supported UMI-style handheld manipulation data collection system.



The category has matured

The original Stanford UMI project proved that handheld data collection can be a powerful way to teach robots from in-the-wild demonstrations.  Since then, the category has expanded. FastUMI redesigned UMI to simplify deployment and reduce hardware-software integration complexity.  UMI-FT added force/torque sensing for force-aware manipulation.  Commercial systems like TRumi and AgileX PiKA now give buyers more productized choices.


Comparison table

Category

DIY Stanford UMI

TRumi

AgileX PiKA

Best for

Open-source research control

Supported UMI-style collection

Multimodal commercial collection

Buyer type

Robotics labs with build capacity

Labs, startups, data teams, enterprise R&D

Teams wanting PiKA’s full ecosystem

Hardware

3D-printed handheld gripper plus GoPro

Engineered handheld TRumi device

PiKA Sense, PiKA Gripper, PiKA Station

Data outputs

UMI repo shows Zarr workflow

Zarr or MCAP through Trossen pipelines

Official page lists rich 6D spatial data, RGB, depth, IMU

Setup burden

Higher DIY burden

Productized and supported

Heavier system integration

Durability

Depends on build quality

CNC-machined metal components, serviceability

Commercial system

Best argument

Maximum openness and flexibility

Practical middle path

Rich multimodal system

Main caution

Build and maintenance burden

Not universal plug-and-play

More complex ecosystem

AgileX describes PiKA as a compact data collection gripper for robotics R&D and lists PiKA Sense, PiKA Gripper, and PiKA Station. The PiKA page states that PiKA Sense is a lightweight handheld unit and PiKA Gripper provides 6D spatial data, RGB imagery, depth, and IMU outputs.


When DIY UMI is the right answer

DIY UMI makes sense when:

Situation

Why DIY fits

You are reproducing the Stanford paper

You need fidelity to the open-source system

You want to modify hardware

Full control matters

You have SLAM and robotics software expertise

Your team can debug the pipeline

You are doing method research

Build effort may be part of the research

The UMI GitHub repo is the right starting point for this path. It provides project, paper, hardware guide, data collection instruction, SLAM repo, installation, and training instructions.


When TRumi is the right answer

TRumi makes sense when your team is past “can we build one?” and has moved to “can we collect data reliably?”


Trossen positions TRumi for teams that need scalable handheld data collection, bimanual and multi-site collection, and robot-specific refinement when needed.  It outputs Zarr or MCAP datasets and uses Trossen Data Collection Pipelines.


TRumi also addresses practical hardware concerns. Trossen lists a cam drive, dual precision linear rails, CNC-machined metal components, embedded identifiers, and constant-force springs.


When PiKA is the right answer

PiKA may make sense when a team wants AgileX’s broader commercial ecosystem, including a handheld data collection unit, robot end effector, and positioning station. AgileX’s product page emphasizes precise indoor and outdoor data collection, embodied AI research, and rich sensor outputs.


A buyer should evaluate PiKA when the desired workflow depends on its multimodal sensor stack, base station approach, or matched handheld and robot-mounted components.


The practical middle path

TRumi’s positioning is the practical middle path:

Problem

TRumi answer

DIY UMI is too fragile or time-intensive

Buy a supported UMI-style system

High-end systems are more than the workflow needs

Use a focused handheld manipulation data collection tool

Data needs structure

Output Zarr or MCAP

Team needs scale

Standardize devices and operator workflow

Robot-specific tuning is still needed

Pair with leader-follower teleoperation


Best for

System

Best for

DIY UMI

Research replication, full customization, open-source control

TRumi

Supported UMI-style data collection, scale, repeatability, Zarr or MCAP output

PiKA

Multimodal commercial collection with PiKA’s ecosystem

Not best for

System

Not best for

DIY UMI

Teams without build, SLAM, or maintenance capacity

TRumi

Teams expecting zero integration or universal robot deployment

PiKA

Teams that want the simplest UMI-style middle path

FAQ

What is the best alternative to building a DIY UMI gripper?

TRumi is the most direct supported UMI-style alternative when the buyer wants a productized handheld manipulation data collection system.


Is TRumi better than UMI?

Not universally. Stanford UMI is an open-source research framework. TRumi is better for teams that value support, durability, repeatability, and productized data workflows.


Is PiKA a UMI alternative?

Yes, PiKA is a commercial data collection gripper system that explicitly tags UMI and Universal Manipulation Interface on its product page.


Does TRumi work with non-Trossen robots?

TRumi data is end-effector-centric rather than tied to one specific joint configuration, but deployment on a target robot still requires integration and validation.


Does TRumi replace PiKA?

No. TRumi and PiKA have different product philosophies. TRumi is a supported UMI-style handheld data collection system. PiKA is a broader commercial system with handheld, end-effector, and station elements.


What does TRumi output?

TRumi outputs Zarr or MCAP datasets through Trossen Data Collection Pipelines.


Should I choose TRumi or leader-follower teleoperation?

Use TRumi for broad handheld collection and leader-follower teleoperation for embodiment-specific refinement and validation.


CTA

Talk to Trossen about your data collection workflow. Tell us whether your team is optimizing for research control, data collection scale, output format, or robot-specific validation.

 
 
 

Comments

Rated 0 out of 5 stars.
No ratings yet

Add a rating

OUR PROMISE TO YOU

We stand behind our products with an industry-leading commitment to reliability, service,
and long-term support—because we believe performance should be measured in years, not months.

BUILT FOR REAL-WORLD RESEARCH ENVIRONMENTS. COVERS DEFECTS IN MATERIALS AND WORKMANSHIP. WEAR COMPONENTS ARE FIELD-REPLACEABLE AND READILY AVAILABLE.
LIFETIME SUPPORT FOR TROSSEN PRODUCTS 

Follow Us On Social

  • LinkedIn
  • Youtube
  • Facebook
  • GitHub
  • Twitter
  • Instagram
  • TikTok

© 2026 Trossen Robotics. All Rights Reserved.

bottom of page