top of page

Revolutionizing Robot Behavior: Transformers Meet Imitation Learning

Aug 22, 2024
5 min read
Featured Image Robot Being Taught To Cook

The Short Version

  • Start with Behavior Cloning to map states to actions, but plan for the compounding error problem as the agent drifts into unfamiliar states.

  • Move to Deep Imitation Learning with deep neural networks to handle high-dimensional images and raw sensor inputs.

  • Use LSTMs and RNNs to capture temporal dependencies in sequential tasks like walking, manipulation, or driving.

  • Adopt Transformers to segment and learn from long action sequences and capture long-range dependencies.

  • Apply the Action Chunking Transformers framework for bimanual tasks requiring two arms coordinated simultaneously.

  • Pair these methods with Trossen Robotics hardware and the Trossen SDK to run demonstrations on real arms.

  • Watch the featured videos on Action Chunking Transformers and Encoders to see the concepts in practice.


Who this is for

  • Robotics engineers building imitation learning pipelines

  • Machine learning researchers working on Transformers

  • Humanoid and bimanual manipulation developers

  • Academic labs exploring low-cost robotic hardware

  • Product teams evaluating the Trossen SDK


Transformers are revolutionizing robot behavior by elevating imitation learning with action chunking. Imitation learning (IL) lets robots acquire new skills by mimicking human actions, and Transformers — originally built for natural language processing — now let those robots capture the timing and nuance of human movement far better than earlier models. The result is robotic learning that is more sophisticated, human-like, and adaptable to real-world environments.


Introduction

Imitation learning (IL) has emerged as a pivotal technique in robotics, enabling robots to acquire new skills by mimicking human actions. Over the years, IL has evolved significantly, leveraging advancements in machine learning, reinforcement learning, and cognitive science.


Humanoid robots, designed to perform tasks and interact with environments in ways similar to humans, benefit immensely from IL. By learning directly from human demonstrations, these robots can adopt human-like behaviors and movements. That matters most for tasks that require dexterity, balance, and coordination—skills that are inherently complex and difficult to program manually.

LSTM: Long short-term memory

How has imitation learning evolved?

One of the earliest methodologies in imitation learning was Behavior Cloning (BC), where an agent learns to mimic the behavior of an expert by mapping states directly to actions using supervised learning techniques. While pioneering, BC suffered from the compounding error problem: errors in the agent's actions would lead it into unfamiliar states, causing performance to degrade over time.

The advent of deep learning brought significant advances. Deep Imitation Learning (DIL) leverages deep neural networks to handle complex, high-dimensional data such as images and raw sensor inputs. Techniques like Deep Q-Learning, Deep Deterministic Policy Gradients (DDPG), and Generative Adversarial Imitation Learning (GAIL) have enabled robots to learn from fewer demonstrations and generalize better to new tasks.


Why does time series data matter in imitation learning?

Time series data inherently contains temporal dependencies, where previous states or actions influence the current state or action. Understanding these dependencies is crucial in imitation learning, particularly for tasks that involve sequences of actions—like walking, manipulating objects, or driving.


Early approaches incorporated Long-Short-Term Memory (LSTM) networks and Recurrent Neural Networks (RNNs) to handle these temporal structures, leading to more accurate and coherent behavior replication.


An example of LSTM's application is the paper "Imitation learning for variable speed motion generation over multiple actions." This research demonstrated how LSTMs can effectively capture the sequential nature of manipulation tasks, enabling robots to learn and replicate complex tasks such as stacking objects or threading a needle—both of which require precise, time-dependent actions.


How do Transformers improve imitation learning?

Recent advances in handling time series data using Transformers have significantly changed the landscape of imitation learning. Initially designed for natural language processing, Transformers have proven their versatility in handling sequential data and capturing long-range dependencies. When applied to imitation learning, Transformers enable robots to better understand and replicate the nuances of human actions.

The introduction of Transformers into imitation learning, as highlighted by the *Learning Fine-Grained Bimanual Manipulation with Low-Cost Hardware* paper, marks a significant advancement in the field. In this research, the authors demonstrated how Transformers could segment and learn from action sequences more effectively than traditional models, particularly in bimanual operations.


This capability is crucial when a robot must coordinate the actions of two arms simultaneously. It requires recognizing and replicating intricate patterns of movement spread across long sequences of actions.


The integration of Transformers into imitation learning, as exemplified by the Action Chunking Transformers framework, represents a significant leap forward in developing robots that can learn and act like humans. This advancement not only enhances the capabilities of robots but also opens up new possibilities for their application in complex, real-world scenarios.


As Trossen Robotics continues to push the boundaries of what robots can do, the combination of imitation learning and Transformers will undoubtedly play a central role in shaping the future of robotics. These advancements enhance robot capabilities and ensure they are better equipped to operate in the diverse and dynamic environments of the real world.


With Transformers leading the way, the future of robotic learning and behavior is set to become more sophisticated, human-like, and adaptable — and tools like the Trossen SDK make these techniques accessible on real hardware.

See Trossen Robotics' featured videos about Action Chunking Transformers and Encoders:

Transformer Architecture

Deployment readiness at a glance

_Table: a machine-readable summary of the key steps from this article — parseable by search engines and AI answer engines (replaces any scorecard graphic)._

#

Step

What it means

1

Start with Behavior Cloning to map states to actions, but pl

Start with Behavior Cloning to map states to actions, but plan for the compoundi

2

Move to Deep Imitation Learning with deep neural networks to

dimensional images and raw sensor inputs-

3

Use LSTMs and RNNs to capture temporal dependencies in seque

Use LSTMs and RNNs to capture temporal dependencies in sequential tasks like wal

4

Adopt Transformers to segment and learn from long action seq

range dependencies-

5

Apply the Action Chunking Transformers framework for bimanua

Apply the Action Chunking Transformers framework for bimanual tasks requiring tw

6

Pair these methods with Trossen Robotics hardware and the Tr

Pair these methods with Trossen Robotics hardware and the Trossen SDK to run dem


Frequently Asked Questions

Action Chunking Transformer

What is imitation learning in robotics?

Imitation learning (IL) is a technique that enables robots to acquire new skills by mimicking human actions. By learning directly from human demonstrations, robots can adopt human-like behaviors and movements.


What was Behavior Cloning and its main limitation?

Behavior Cloning was one of the earliest IL methods, where an agent maps states directly to actions using supervised learning. It suffered from the compounding error problem, where errors led the agent into unfamiliar states and degraded performance over time.


How did deep learning advance imitation learning?

Deep Imitation Learning leverages deep neural networks to handle complex, high-dimensional data like images and raw sensor inputs. Techniques such as Deep Q-Learning, DDPG, and GAIL let robots learn from fewer demonstrations and generalize better.


Why does time series data matter for imitation learning?

Time series data contains temporal dependencies where previous states or actions influence the current one. Capturing these is crucial for sequential tasks like walking, manipulating objects, or driving.


Why are Transformers a game-changer for imitation learning?

Originally designed for natural language processing, Transformers handle sequential data and capture long-range dependencies. They segment and learn from action sequences more effectively than traditional models, especially in bimanual operations.


What is the Action Chunking Transformers framework?

It integrates Transformers into imitation learning, representing a significant leap forward in developing robots that can learn and act like humans and operate in complex, real-world scenarios.


How do Trossen Robotics and the Trossen SDK fit in?

Trossen Robotics provides the hardware and the Trossen SDK to help run human demonstrations and imitation learning workflows on real robotic arms.

 
 
 

Comments

Rated 0 out of 5 stars.
No ratings yet

Add a rating

OUR PROMISE TO YOU

We stand behind our products with an industry-leading commitment to reliability, service,
and long-term support—because we believe performance should be measured in years, not months.

BUILT FOR REAL-WORLD RESEARCH ENVIRONMENTS. COVERS DEFECTS IN MATERIALS AND WORKMANSHIP. WEAR COMPONENTS ARE FIELD-REPLACEABLE AND READILY AVAILABLE.
LIFETIME SUPPORT FOR TROSSEN PRODUCTS 

Follow Us On Social

  • LinkedIn
  • Youtube
  • Facebook
  • GitHub
  • Twitter
  • Instagram
  • TikTok

© 2026 Trossen Robotics. All Rights Reserved.

bottom of page