top of page

YOUR PHYSICAL AI PARTNER

PHYSICAL AI DATA COLLECTION PLATFORMS:
Hardware, SDK, and Cloud Built to Scale Robot Data

Built for data collection labs and machine learning teams. Teleoperate, record, review, and scale your robot learning data on one connected system, from a single station to many. No one-off rigs, no custom engineering bottlenecks.

​

Trossen is a complete platform for physical AI data collection: the hardware is paired with the SDK and Trossen Cloud, so you spend your time collecting data instead of integrating tools.

Data Collection 1.png

YOUR PHYSICAL AI PARTNER

PHYSICAL AI 
DATA COLLECTION PLATFORMS:

Hardware, SDK, and Cloud Built to Scale Robot Data

Built for data collection labs and machine learning teams. Teleoperate, record, review, and scale your robot learning data on one connected system, from a single station to many. No one-off rigs, no custom engineering bottlenecks.

​

Trossen is a complete platform for physical AI data collection: the hardware is paired with the SDK and Trossen Cloud, so you spend your time collecting data instead of integrating tools.

WHY DATA COLLECTION ORGANIZATIONS CHOOSE TROSSEN

Data Collection 2.png

BUILT TO KEEP COLLECTING DATA

RELIABILITY

In a data collection campaign, every hour a robot is down is an hour of demonstrations you don't collect. Trossen hardware is built so a worn part is a quick fix, not a lost week: field-replaceable parts and cable swaps in minutes, and we stock the parts.

​

Every arm has an industrial controller with a built-in touchscreen for setup and diagnostics, locking M12 connectors instead of USB, and a slewing bearing in the base, so the arm is built for long collection sessions.

​

When you need help, you reach our team by email, support ticket, or a shared Slack channel, with video calls when something needs a closer look. We reply within 24 business hours, and the hardware carries a one-year limited warranty and lifetime product support.

FROM ONE STATION TO MANY

SCALE QUICKLY

Collecting enough data usually means running more than one station, and that is where one-off rigs break down. Workbench and Rivet are standardized, repeatable stations, so every new one starts from the same known setup instead of another custom build.

​

Workbench puts two WidowX arms on a standardized mounting plate with fixed arm and camera geometry, so every session starts from the same setup. Rivet adds a mobile base with a vertical axis and a swappable battery, so you can collect indoors across locations and heights.

​

Choose WidowX Core, Pro, or Heavy arms to match your peak payload and reach, and run the same Trossen SDK across every station. Scaling your dataset doesn't mean scaling your engineering team. Adding another station means ordering one, not engineering one.

SMOOTH TELEOP MEANS CLEAN TRAINING DATA

BETTER DATA WITH GLIDE

Your model can only be as clean as your demonstrations. Glide is a lightweight leader arm built to record clean demonstrations for imitation learning, so the motion your operator makes is the motion that ends up in the dataset.

​

Its encoder-only main joints are designed for stiction-free teleoperation, with no servos in the main joints to add stiction, cogging, or low-speed judder to your recordings. A spring-based mechanism balances the arm, designed to keep long collection sessions comfortable.

​

Left and right handed versions match the operator's hand, carbon fiber links keep the arm light, and the handle puts a joystick, a trigger, and programmable buttons at the operator's fingertips.

​

Checkout Glide

YOUR OPERATOR, WHEREVER THEY ARE

TELEOP, ANYWHERE IN THE WORLD

Operators can run a robot remotely over the internet, so you aren't limited to the people in the room with the robot. It works with the Rivet mobile base and with Glide leader arms on Cockpit.

​

The setup is the same locally or remotely: Glide leader arms on a Cockpit operator station control the robot, and the Glide joystick drives Rivet's mobile base and vertical axis. Cockpit is a portable, wheeled stand for one or two Glide arms, so an operator can work next to the robot or from another location.

​

The robot stays in the task area while the operator works from wherever is convenient, so your hardware keeps collecting and you can bring in skilled operators from outside your lab. Every demonstration they record adds to your dataset.

THE TOTAL PHYSICAL AI PIPELINE

CLOUD SOLUTIONS

Store, review, and improve your data in one place.

HARDWARE + SDK + CLOUD
One connected system for physical AI data collection, from the first recording to model development.

HARDWARE

PLUG IN AND COLLECT

​

Take your arms out of the box, plug them in, and connect to Trossen Cloud with an access code. You're collecting data to the cloud within half an hour.

​

GROW IT YOU WAY

​

WidowX arms, the Workbench station, the mobile Rivet base, and Glide leader arms on Cockpit all work together, so you can add hardware as your data collection grows. Already have arms? Build with what you have: the SDK is open-source with Python bindings, and Rivet is available as a base with no arms so you can mount your own. Integration with third-party arms is up to you.

SDK

OPEN-SOURCE, WITH PYTHON BINDINGS

​

The SDK records robot and camera data with high-resolution timestamps, so the streams can be synchronized after collection.

​

Start collecting without a deep dive into the SDK.

TROSSEN CLOUD

Trossen Cloud is where your recorded robot learning data goes next, before model training. Connect your hardware and collect data straight to it, then use the dataset and data quality workbench to open an episode, watch the video, and see how good the data is and what's wrong with it.

​

Your data is encrypted at rest and it is yours: it isn't deleted if you leave. Early access users use Trossen Cloud free today, and on the roadmap are tools to clean, store, and eventually resell your data.

CHOOSE YOUR HARDWARE FOR DATA COLLECTION

READY TO SCALE UP YOUR 
PHYSICAL AI PIPELINE?

Stop troubleshooting custom rigs. Let's talk about your lab's data targets and

get a standardized collection system to your team.

Thank you! Our team will reach out to you soon!

OUR PROMISE TO YOU

We stand behind our products with an industry-leading commitment to reliability, service,
and long-term support—because we believe performance should be measured in years, not months.

BUILT FOR REAL-WORLD RESEARCH ENVIRONMENTS. COVERS DEFECTS IN MATERIALS AND WORKMANSHIP. WEAR COMPONENTS ARE FIELD-REPLACEABLE AND READILY AVAILABLE.
LIFETIME SUPPORT FOR TROSSEN PRODUCTS 

Follow Us On Social

  • LinkedIn
  • Youtube
  • Facebook
  • GitHub
  • Twitter
  • Instagram
  • TikTok

© 2026 Trossen Robotics. All Rights Reserved.

bottom of page