LITE
THE SAME STATION,
NO ONBOARD COMPUTE
Starting at $1,495
Academic/Startup: $1,196
A lighter, lower-cost two-arm bimanual station: two WidowX arms on a compact mount, without onboard compute or a screen. Ships with an RealSense D405 camera mount, cameras themselves are an add-on. A good fit if you're supplying your own compute or want a leaner build.

THE BIMANUAL STATION THAT MOVES WITH THE WORK
CHOOSE YOUR CONFIGURATION
PRICING

ALL THE DETAILS
SPECIFICATIONS
Measurements for integration and hardware sizing.
INTEGRATIONS
Workbench is the fixed two-arm embodiment on the Trossen platform. The arms are our next-generation WidowX followers, teleoperated from a pair of Glide leader arms at a Cockpit station, and driven by the same open-source Trossen SDK. Pick the payload your task needs and nothing else about how you work has to change.
CONTROLLERS & SOFTWARE
The hardware is only half the story.
A TWO-ARM STATION THAT MOVES WHEN YOUR WORK DOES
COMING SOON.......................
A bimanual setup built on one table stays on that table. Workbench is one station you can lift. Two WidowX deployment arms and three cameras, one on each wrist and one scene camera on the built-in stem, share a machined metal plate with built-in handles, so the whole station travels as a single piece. Set it on a new bench, clamp it down, and run one calibration routine instead of unmounting the arms, re-measuring the spacing, and rebuilding a frame on the other side of the room. Workbench arrives fully set up. The plate, clamps, camera stem, all three cameras, onboard NVIDIA Jetson AGX Orin 64 GB compute, power, UI, and networking all ship with it, ready to run. Already have your own cameras and computer? Workbench Lite is a separate product with the same plate, stem, and arms, without cameras or compute.


Trossen AI Hardware and Kits
Are you interested in obtaining a quote? Fill out the form, and we will contact you soon.
Ship Address*
Bill Address*
Never share sensitive information (credit card numbers, social security numbers, passwords) through this form.