top of page

What Is a Robotics Operating System? A Guide

Sep 11
22 min read

Modern artificial intelligence thrives on real-world data. To teach a robot how to perform a task, you need to capture its movements, sensor readings, and camera feeds in a perfectly synchronized way. This is where the Robot Operating System (ROS) becomes an essential tool for AI and machine learning. It acts as the central nervous system for data collection, providing the infrastructure to connect physical hardware with your ML training pipelines. This robotics operating system makes it possible to record rich, multi-modal datasets from teleoperation sessions, giving you the high-quality information needed to train the next generation of intelligent, embodied AI systems.

Key Takeaways

  • ROS is a framework, not an operating system

    : It acts as the middleware that connects your robot's hardware and software, allowing different programs (nodes) to communicate seamlessly through a standardized messaging system.

  • Accelerate your work with a rich ecosystem

    : Instead of starting from scratch, you can use a vast library of open-source packages, powerful simulation (Gazebo) and visualization (RViz) tools, and get help from a massive global community.

  • Choose ROS 2 for modern robotics and AI

    : For any new project, start with ROS 2. It offers the reliability, security, and real-time control needed for commercial applications and for collecting the high-quality, synchronized data required to train AI models.

What Is a Robotics Operating System (ROS)?

If you've ever wondered how a complex robot with dozens of sensors, motors, and processors all work together, the answer is often ROS. Standing for Robot Operating System, ROS is an open-source collection of software libraries and tools that help developers build robot applications. Think of it as the software glue that connects all of a robot's different parts, from its cameras and arms to the algorithms that make it smart. It provides a standard way for all these components to communicate and work in harmony.

Instead of starting from scratch every time you build a robot, ROS gives you a foundation to build upon. It handles many of the common challenges in robotics, like making a sensor's data available to a motor controller or visualizing what the robot is "seeing" in a 3D environment. This lets researchers, students, and engineers focus on creating new and interesting robot behaviors instead of reinventing the wheel.

How ROS Differs from a Standard OS

First things first: despite its name, ROS is not an operating system like Windows, macOS, or Linux. In fact, it runs on top of a standard OS, most commonly a version of Linux like Ubuntu. It’s more accurate to call ROS "middleware." Think of it as a universal translator that sits between the robot's hardware, the main operating system, and all the different software programs you write.

This middleware approach is what makes ROS so powerful. It creates a communication layer that allows separate programs, called "nodes," to talk to each other seamlessly. For example, a node processing data from a camera can easily publish that information, and another node controlling the robot's wheels can subscribe to it to react. This modular structure simplifies development and makes it easy to build robot programs piece by piece.

Why the Name "Operating System" Can Be Misleading

So if it's not a true OS, why the name? The "Operating System" title was chosen because ROS provides many services that are similar to what a traditional OS does for a computer. It helps manage processes, handles communication between programs, and provides a standard way to interact with hardware. It essentially creates an organized ecosystem for all your robot's software to live in.

The Robot Operating System gives developers a common language and a set of rules for building applications. This includes tools for low-level device control, message-passing between different software modules, and hardware abstraction, which lets you write code that isn't tied to one specific brand of sensor or motor. This flexibility means you can pick and choose the tools you need, making it a highly adaptable framework for almost any robotics project.

How Does ROS Work?

ROS organizes a robot's software into a network of independent programs. This modular approach makes it easier to build, test, and manage complex robotic behaviors. Instead of writing one giant, monolithic program, you create small, reusable pieces that communicate with each other. This structure is the key to how ROS simplifies robotics development. It provides the "plumbing" that connects all the different software components, from sensor drivers to high-level planning algorithms, into a single, cohesive system. Let's look at the three core concepts that make this possible: nodes, topics, and the master.

Meet the Nodes: The Core of ROS

Think of a robot as a team of specialists. One specialist handles vision, another manages movement, and a third plans the route. In ROS, these specialists are called "nodes." A node is simply a program responsible for a single, specific task. For example, you might have one node that reads data from a camera, another that controls the wheel motors, and a third that processes sensor information to avoid obstacles. These nodes are the fundamental building blocks of any ROS application. By breaking down a complex robotic system into these small, manageable pieces, ROS makes it much easier to develop, debug, and reuse code.

How Robots Talk: Topics, Messages, and Services

So, if you have all these individual nodes running, how do they work together? They communicate through a system of "topics" and "messages." It works like a public announcement system. A node can "publish" a message to a specific topic, and any other node that "subscribes" to that topic will receive it. For instance, a camera node might continuously publish image data to a topic called . A separate image processing node can then subscribe to that topic to get the latest frames. This publish-subscribe model allows different parts of your robot to share information without being directly connected, making the whole system incredibly flexible. For more direct interactions, ROS also offers "services," which let one node send a request to another and wait for a direct response.

The ROS Master and Why ROS 2 Is Different

In the original version, ROS 1, all this communication was managed by a central program called the ROS Master. You can think of it as a switchboard operator that helps nodes discover each other and establish connections. While this worked well, it also created a single point of failure; if the Master went down, the entire system could stop communicating. This is one of the biggest changes in ROS 2. The newer version gets rid of the central Master and uses a decentralized discovery process. This makes ROS 2 far more robust and reliable, especially for complex applications like multi-robot systems or commercial products where you can't afford downtime. This change is a key reason why modern AI robotics platforms are increasingly built on ROS 2.

Why Do So Many Developers Use ROS?

If you've spent any time in the robotics world, you've heard developers, researchers, and students talk about ROS. There's a good reason it has become the go-to framework for so many projects. At its heart, ROS is more than just software; it's a massive ecosystem of tools, libraries, and conventions designed to make your life as a robot builder much, much easier. It helps you avoid reinventing the wheel so you can focus on the truly innovative parts of your work.

Think of it as a set of building blocks. Instead of starting from scratch every time you build a new robot, ROS gives you a standardized way to handle common tasks like hardware abstraction, communication between different software modules, and package management. This modular approach means you can build complex systems more quickly and reliably. Whether you're a student building your first robot or a corporate R&D team prototyping a new AI-driven system, ROS provides a solid foundation that scales with your ambitions. It’s packed with features that streamline development, from powerful simulation tools to a global community ready to help.

Run Your Code on Different Robots

One of the most powerful features of ROS is its emphasis on modularity. It encourages you to write your code in small, independent programs called nodes. Because these nodes communicate through a standardized system, you can often reuse them across completely different robots with few, if any, changes. Imagine you’ve written a brilliant algorithm for a robotic arm to pick up an object. With ROS, you can take that same code and adapt it for a different arm or even a mobile manipulator without having to start over.

This principle of reusability is a game-changer. It saves countless hours of development time and allows you to build on your previous work. You can develop a navigation stack on a small, wheeled robot and later apply it to a larger, more complex mobile AI platform. This flexibility lets you focus on improving your algorithms instead of rewriting basic functionality for every new piece of hardware.

Test in Simulation with Gazebo

Before you let your new robot roam free, you need to know its code works. But testing on physical hardware can be risky and expensive. What if there’s a bug that causes your robot to crash into a wall or damage its own arm? This is where simulation comes in, and ROS has one of the best tools for the job: Gazebo. Gazebo is a 3D physics simulator that lets you create a virtual twin of your robot and its environment.

You can test your algorithms in this digital playground, spotting bugs and refining performance in a safe, controlled setting. Because Gazebo is tightly integrated with ROS, the code you run in the simulation is the same code you'll deploy on the real robot. This makes it an essential tool for everything from debugging simple movements to training complex AI behaviors. You can simulate your robot's interactions with the world, ensuring everything works as expected before you ever power on the physical hardware.

Visualize Your Robot's World with RViz

A robot running complex code can feel like a black box. You know it's processing data from its sensors, but what is it actually "seeing" or "thinking"? RViz is the tool that opens up that box. It’s a 3D visualization environment that gives you a real-time window into your robot's mind. With RViz, you can see all the data streams flowing through your ROS system in an intuitive, graphical way.

You can overlay a camera feed on a 3D model of the world, watch the points from a LiDAR sensor appear in real-time, or see the path your navigation algorithm is planning for the robot to follow. This visual feedback is incredibly valuable for debugging. Instead of trying to interpret thousands of lines of numerical data, you can instantly see if your robot's perception of a wall matches its actual location. It’s an indispensable tool for anyone working with sensor data and robotic perception.

Access a World of Open-Source Packages

Why build something from scratch when an expert has already built it and shared it for free? This is the philosophy at the core of the ROS ecosystem. Because ROS is open source, it has fostered a vibrant community that has created thousands of free software packages. These packages provide ready-to-use solutions for an enormous range of robotics tasks, from controlling specific hardware to implementing cutting-edge algorithms.

Need a driver for a new camera or a motor controller? There's probably a ROS package for it. Looking for a state-of-the-art algorithm for simultaneous localization and mapping (SLAM)? You can find several to choose from. This vast library of code allows you to assemble sophisticated robotic systems quickly. You can explore available packages and integrate them into your project, letting you stand on the shoulders of the global robotics community and focus on what makes your project unique.

Lean on a Massive Community and Great Docs

Getting started with a new, complex framework can feel intimidating, but with ROS, you're never on your own. One of its greatest strengths is the massive and active community surrounding it. From detailed tutorials and official documentation to bustling forums and user groups, there is a wealth of resources available to help you learn and solve problems. If you get stuck, chances are someone has faced the same issue and a solution is just a quick search away.

This supportive environment makes ROS accessible to everyone, from students just beginning their robotics journey to seasoned engineers tackling difficult research problems. The community maintains extensive documentation and provides support through platforms like the ROS Discourse forum, where you can ask questions and share your own discoveries. This collaborative spirit is what has helped ROS grow into the powerful, practical tool it is today.

ROS 1 vs. ROS 2: What's New and Why It Matters

As the robotics community grew, the limitations of the original ROS (now called ROS 1) became clear. It was a groundbreaking framework, but it wasn't built for the complex, multi-robot systems and commercial applications that are becoming common today. In response, the community rebuilt it from the ground up to create ROS 2. Think of it less as an update and more as a complete sequel designed for the future of robotics. Understanding the key differences will help you decide which one is right for your project.

Better Support for Real-Time Control

If your robot needs to react to the world instantly and predictably, you need real-time control. This is essential for tasks like delicate manipulation or high-speed navigation where a millisecond delay can cause a failure. ROS 1 struggled with this; its scheduler couldn't guarantee that a critical command would run at a precise moment, which is a dealbreaker for commercial or safety-critical products. In contrast, ROS 2 was created to handle real-time tasks from the ground up. It gives developers fine-grained control over when and how code executes, allowing for deterministic behavior. This makes it a much better choice for performance-critical applications where reliability and predictability are non-negotiable.

A New Standard for Communication (DDS)

In ROS 1, all nodes had to connect to a central "ROS Master" to find each other. If that single master node went down, the whole system stopped communicating. This single point of failure is a major risk in complex or long-running applications. ROS 2 gets rid of this problem by using a new communication system called the Data Distribution Service (DDS). DDS is a robust, peer-to-peer industry standard used in everything from aerospace to industrial control. It allows nodes to discover each other automatically and communicate directly, resulting in a more resilient, flexible, and scalable messaging system for your robot.

Stronger Security and a More Modular Design

ROS 1 was created in a research setting and had very few security features, leaving it vulnerable on open networks. Recognizing this, ROS 2 was designed with security in mind, giving you tools for encryption, authentication, and access control. Beyond security, the architecture of ROS 2 is also far more modular. You can swap out core components, like the DDS implementation or memory allocators, to better suit your project's specific needs. This flexibility allows you to build a more efficient and customized system without having to reinvent the wheel, which is perfect for specialized research or product development.

Which Version Should You Use?

So, which one is for you? While many older projects and tutorials still use ROS 1, the answer for any new development is clear: use ROS 2. The improvements in performance, reliability, security, and flexibility make it the superior choice for modern robotics. The entire community is focused on ROS 2, and it's where all the exciting new development is happening. For anyone building systems for research, AI data collection, or commercial applications, ROS 2 is recommended for new developments. That's why our AI-ready platforms are built to support ROS 2, giving you a solid foundation for your work from day one.

What Can You Build with ROS?

The better question might be, what can't you build? Because ROS is a flexible framework rather than a rigid program, you can use it as the foundation for almost any robotics project you can imagine. It provides the essential plumbing for communication, control, and data processing, letting you focus on the unique parts of your project. From university research projects to industrial automation prototypes, ROS gives you the tools to bring your ideas to life. Whether you're building a robot that sorts objects or one that explores a new environment, ROS provides a solid starting point.

Build and Control Robotic Arms

If you want to build a robot that can pick up, move, or interact with objects, ROS is an invaluable tool. It offers powerful software packages for manipulation that handle the complex math behind robot arm movement. For example, the popular MoveIt! framework helps with motion planning, kinematics, and collision avoidance, so you don't have to write that code from scratch. This means you can tell your robot arm what to do (like "pick up that block") and MoveIt! helps figure out how to do it safely. This allows you to get a platform like a WidowX arm performing complex tasks much faster.

Create Autonomous Mobile Robots

ROS is the go-to framework for creating robots that move around on their own. It provides a complete software stack for autonomous movement that handles the core challenges of mobility. Using ROS packages, your robot can build a 2D or 3D map of its surroundings (mapping), determine its own position within that map (localization), and calculate a path to a goal while avoiding obstacles (path planning). This is the same fundamental technology used in everything from warehouse robots to autonomous research vehicles. With ROS, you can equip a mobile robotics platform with sensors and get it moving around a room with surprising speed.

Enable Remote Control and Data Capture

ROS is perfect for teleoperation, which is just a technical term for controlling a robot remotely. More importantly, it excels at capturing data during that remote control. You can use a joystick or other input device to guide a robot through a task, and ROS can record every single detail: the operator's commands, the robot's joint movements, and the video feed from its cameras. This synchronized, multi-modal data is exactly what you need for training modern AI models through imitation learning. This workflow is so important that it's a core feature of systems like our robotic data collection tools.

Integrate Cameras, Sensors, and More

A robot is only as smart as the data it receives. ROS makes it incredibly easy to add new sensors and peripherals to your system. Its modular, node-based architecture means you can add a camera, a LiDAR scanner, a force-torque sensor, or a microphone just by running a new node. That node publishes its data on a ROS topic, and any other part of your system can subscribe to it. This "plug-and-play" capability allows you to build robots with a rich perception of the world. You can start with a simple AI-ready research kit and continuously add new capabilities as your project evolves, without having to rebuild your entire software stack.

How ROS Powers AI and Machine Learning

ROS is more than just a framework for controlling robots; it’s a powerful engine for modern AI and machine learning development. If you want to train a robot to perform a task, you first need high-quality data from the real world. ROS provides the essential plumbing to collect, synchronize, and stream that data, turning your robot into a powerful tool for building intelligent systems. It bridges the gap between physical hardware and the data-hungry algorithms that drive embodied AI.

Connect ROS to Your ML Pipeline

Think of ROS as a helpful middleman that helps different parts of your robot’s software communicate. It’s built on a system of nodes, which are small, individual programs that handle specific jobs, like reading a sensor or controlling a motor. These nodes are organized into ROS packages, which act like folders for your robot's code. This modular structure makes it incredibly easy to connect your robot's data streams directly into a machine learning pipeline. You can create a node that captures camera images and another that records joint positions, then send that data straight to a system for training.

Capture Rich, Multi-Modal Data for Training

Modern AI models thrive on diverse, multi-modal data, which means information from multiple sources, like cameras, microphones, and force sensors. ROS uses a graph-based system where nodes can send and receive information through messages. This architecture is perfect for capturing synchronized data streams. For example, you can record a video feed, the robot arm’s exact movements, and the force being applied by its gripper all at the same time. This rich, layered data is exactly what you need to teach a robot complex manipulation tasks through imitation or reinforcement learning. Our Data Collection SDK is designed to simplify this process, helping you build structured datasets for your AI models.

Build Cloud-Connected Robot Fleets

Training robust AI models often requires data from more than one robot, sometimes from an entire fleet. ROS 2 was specifically designed to support these kinds of distributed systems. It was built to handle real-time tasks and work across different computer systems, making it well-suited for cloud-connected applications and managing multiple robots at once. You can deploy a fleet of robots to collect data in parallel, send that information to the cloud for processing, and then deploy updated models back to the robots. This scalable approach is essential for developing AI that can operate reliably in complex, real-world environments.

Let's Clear Up Some Common ROS Myths

ROS is an incredibly powerful tool, but its reputation can sometimes make it feel a bit intimidating. If you're just getting started, you've probably heard a few things that gave you pause. Is it a full-blown operating system? Do you need a PhD in computer science to use it? Is it even reliable enough for a real project?

Let's take a moment to clear the air. A lot of the common concerns about ROS come from simple misunderstandings. By breaking down these myths, you can approach your next robotics project with more confidence and a clearer understanding of what ROS really is: a flexible framework designed to make your life easier.

Myth: ROS Is a Complete OS Like Linux

One of the most common points of confusion comes from the name itself. While it's called the Robot Operating System, ROS is not an operating system in the same way as Windows, macOS, or Linux. It doesn't manage your computer's core functions like memory or file systems. Instead, ROS is a flexible framework that runs on top of a host OS, which is usually Ubuntu Linux.

Think of it as a meta-operating system or middleware. It provides a set of software tools and frameworks that add robot-specific features to a standard OS. This includes things like hardware abstraction, so you don't have to write custom code for every sensor, and a communication system that lets different parts of your robot's software talk to each other seamlessly.

Myth: You Need to Be an Expert to Use ROS

It's true that ROS has a learning curve, but you definitely don't need to be a robotics expert to get started. In fact, ROS was created to do the opposite: to lower the barrier to entry. It handles a lot of the foundational, repetitive work for you. This allows you to focus on making robots smarter and building unique applications, rather than reinventing the wheel.

With ROS, you can pull from a massive library of open-source packages for tasks like navigation, manipulation, and perception. Platforms like our AI-ready research kits come with ROS pre-installed and configured, so you can jump straight into developing your application without getting bogged down in setup.

Myth: ROS 1 and ROS 2 Are Interchangeable

This is a critical point to understand before starting a new project. ROS 2 is not just an update to ROS 1; it's a complete, ground-up redesign. The two versions are not compatible with each other out of the box. You can't simply run a ROS 1 node with a ROS 2 system without using a special bridge, which can add complexity.

ROS 2 was developed to address some of the limitations of ROS 1, particularly for commercial products and complex systems. It offers better security, support for real-time tasks, and a more robust communication system. While ROS 1 is still widely used in research, ROS 2 is the new standard for modern robotics development. Choosing between them depends on your project's specific needs and the existing tools you plan to use.

Myth: Open-Source Means It's Unstable

The term "open-source" sometimes gets an unfair reputation for being hobbyist-grade or unreliable. For ROS, the opposite is true. Because ROS is open source, its code is constantly being reviewed, tested, and improved by a global community of thousands of developers, researchers, and engineers. This collaborative environment often makes the software more robust, not less.

Bugs are typically found and fixed quickly, and the framework is battle-tested in countless academic and commercial applications, from warehouse automation to autonomous vehicles. The open nature of ROS is one of its greatest strengths. It fosters a rich ecosystem of shared knowledge, free packages, and community support that you just can't find in a closed, proprietary system.

Common Challenges When Working with ROS

Let’s be honest: for all its power, getting started with ROS can feel like a big undertaking. It’s an incredibly deep and flexible framework, but that same depth can present a few hurdles when you’re just starting out. It’s helpful to know what these common challenges are so you can be prepared to meet them head-on.

Think of these not as roadblocks, but as rites of passage. Every seasoned robotics developer has spent time untangling dependencies or staring at a terminal trying to figure out why a node isn’t behaving. The good news is that the ROS community has built an amazing set of tools to help you through it. Understanding the learning curve, managing how different software pieces fit together, and learning how to debug a distributed system are the three key skills that will help you move from a beginner to a confident ROS developer. We’ll walk through each one so you know what to expect and how to get through it.

Tackle the Learning Curve

The first thing you'll notice about ROS is that it's huge. With thousands of packages in the ecosystem, it’s easy to feel overwhelmed. The key is to remember that you don't need to learn everything at once. The best way to approach ROS is with a specific project in mind. Instead of trying to understand the entire navigation stack, for example, just focus on what you need to get your robot moving from point A to point B.

Start small and build on your successes. The official ROS Tutorials are an excellent, hands-on starting point. Work through them to get a feel for the core concepts. Once you have the basics down, you can start exploring packages that are relevant to your project, whether it’s for manipulation, computer vision, or something else entirely.

Handle Dependencies and Versioning

ROS projects are built from many different software packages that rely on each other to work. This modularity is a strength, but it can also create headaches with dependencies and versioning. You might find a great package for object detection, only to realize it depends on a different version of a library you’re already using. This is a classic software development problem, but it’s especially common in the sprawling ROS ecosystem.

This is where using a standardized platform can save you a ton of time and frustration. When you work with integrated systems, like our AI-ready research kits, the environment is pre-configured and validated. This lets you skip the tedious setup and focus on your actual research or application. If you are building from scratch, tools like Docker can also help create consistent, reproducible environments for your projects.

Debug a Complex, Distributed System

When your robot doesn’t do what you expect, figuring out why can be tricky. Because ROS is a distributed system, a dozen different programs, or nodes, might be running and communicating simultaneously. The problem might not be in the code you’re looking at, but in a separate node that’s sending faulty data or no data at all. Tracing the source of an error requires a different approach than debugging a single, self-contained program.

Thankfully, ROS provides a whole suite of visualization and inspection tools to help you peek under the hood. Tools like RViz are invaluable for seeing what your robot’s sensors are seeing and visualizing its internal state. You can use to get a live map of how all your nodes are connected and what messages they’re passing. Learning to use these tools effectively is the key to debugging efficiently and keeping your project moving forward.

How to Get Started with ROS

Jumping into a framework as powerful as ROS can feel like a huge undertaking, but it doesn't have to be. The best way to approach it is by breaking the process down into a few practical steps. You don’t need to become a ROS expert overnight. Instead, you can focus on getting a simple system up and running, which gives you a solid foundation to build on. The key is to start with the right tools so you can spend less time on basic configuration and more time on the fun part: making your robot do interesting things.

Getting started really comes down to three main areas. First, you need the physical robot itself. Second, you need the software and the knowledge to use it. And third, you can find integrated platforms that bundle the hardware and software together to give you a major head start. By tackling these one at a time, you can create a clear path for yourself, whether you're a student building your first project, a researcher prototyping a new idea, or an engineer developing a system for data collection. Let's walk through what you need for each step.

Find the Right Hardware

Your first step is choosing the physical robot. The good news is that you don't have to build one from scratch. A huge variety of robots are already designed to work with ROS, from large industrial arms to smaller, more accessible research robots. The most important thing is to select hardware that is well-supported and comes with clear documentation. This is why many developers and researchers begin with modular stationary AI platforms that are built specifically for ROS integration. Starting with a robot that’s already compatible saves you from the headache of writing low-level hardware drivers and lets you focus on your application right away.

Get the Right Software and Training

Once you have your hardware, it's time to get the software and learn how to use it. ROS is a collection of free, open-source software tools, and one of its greatest strengths is its massive and active community. You are never truly on your own. The official ROS website is your home base for everything you need, including extensive documentation, tutorials, and forums. If you get stuck, you can ask questions on the Robotics Stack Exchange or join a chat. This community support system is invaluable, especially when you're just starting out, as it provides a safety net of experts who are happy to help you solve problems.

Find ROS-Ready Robots and Platforms

If you want to move even faster, you can skip much of the manual setup by using a ROS-ready platform. Unlike buying individual components, a platform provides an integrated system where the hardware and software are already configured to work together. These AI-ready kits often come with ROS pre-installed and include useful packages for common tasks, like MoveIt for motion planning or Nav2 for navigation. This approach is perfect for teams that want to focus on developing AI models or automation workflows instead of spending weeks just getting their robot to move. It turns the robot into a tool you can use immediately, not a project you have to build first.

Frequently Asked Questions

Do I need a computer science degree to use ROS? No, absolutely not. While ROS is a deep and powerful framework, it was actually created to make robotics more accessible. It handles a lot of the complex, low-level work for you so you can focus on what you want your robot to do. The community provides excellent tutorials that walk you through the basics step-by-step. If you have some programming experience and a willingness to learn, you have everything you need to get started.

Should I start a new project with ROS 1 or ROS 2? For any new project, you should use ROS 2. While many older projects and tutorials use ROS 1, the entire robotics community is now focused on ROS 2. It was redesigned from the ground up to be more reliable, secure, and capable of handling the demands of modern commercial and multi-robot systems. Starting with ROS 2 ensures your project is built on a modern foundation that will be supported for years to come.

What's the most common setup for running ROS? The vast majority of ROS development happens on a computer running Linux, specifically a version of Ubuntu. While it's possible to use it on other operating systems, sticking with the recommended Ubuntu version for your chosen ROS distribution will make your life much easier. This consistency means that community-provided packages and tutorials will work right out of the box, saving you a lot of troubleshooting time.

Is ROS just for academic research, or is it used in commercial products? While ROS has its roots in academic research, it has grown far beyond the university lab. ROS 2, in particular, was developed with commercial needs in mind, adding features for security, real-time control, and reliability. You can find it running in everything from warehouse logistics robots and autonomous vehicles to advanced manufacturing systems. It has become a proven, industry-standard framework for building serious robotic applications.

My team focuses on machine learning, not robotics. How can ROS help us? This is a great question because it gets to the heart of modern AI development. Your machine learning models need high-quality, real-world data to learn from, and ROS is the perfect tool for collecting it. It allows you to use a robot as a sophisticated data capture device, recording synchronized streams of video, joint movements, and sensor readings as it performs a task. This gives you the structured, multi-modal datasets you need to train powerful embodied AI models.

 
 
 

Comments

Rated 0 out of 5 stars.
No ratings yet

Add a rating

OUR PROMISE TO YOU

We stand behind our products with an industry-leading commitment to reliability, service,
and long-term support—because we believe performance should be measured in years, not months.

BUILT FOR REAL-WORLD RESEARCH ENVIRONMENTS. COVERS DEFECTS IN MATERIALS AND WORKMANSHIP. WEAR COMPONENTS ARE FIELD-REPLACEABLE AND READILY AVAILABLE.
LIFETIME SUPPORT FOR TROSSEN PRODUCTS 

Follow Us On Social

  • LinkedIn
  • Youtube
  • Facebook
  • GitHub
  • Twitter
  • Instagram
  • TikTok

© 2026 Trossen Robotics. All Rights Reserved.

bottom of page