top of page

Trossen AI Arms Are Now Integrated Into OpenPI for VLA Models

Dec 3, 2025
6 min read

The Short Version

  • Clone the dedicated OpenPI fork with Trossen AI Stationary Kit support to get started.

  • Collect episodes on Trossen AI arms using LeRobot for real-world tasks.

  • Fine-tune π₀ or π₀.₅ policies using the integrated training and inference workflows.

  • Connect Hugging Face for datasets and checkpoints.

  • Run inference on your robot directly from the OpenPI client.

  • Follow the complete integration guide for setup, hardware tips, and example configurations.

  • Evaluate policies and refine your setup as new benchmarks and tools ship.


Who this is for

  • Robotics researchers

  • ML and embodied AI developers

  • Robotics startups

  • VLA model engineers

  • Physical Intelligence framework users


In our previous blog post, we explored how we successfully ran zero-shot inference using Pi Zero (π₀) on our Aloha Kit, showing that state-of-the-art foundation models could transfer to real-world robotic hardware. That experiment was the start of something bigger.

Today, we’re taking the next step: Trossen AI arms are now fully integrated into the OpenPI framework. This means you can now collect data, fine-tune policies, and deploy cutting-edge vision-language-action (VLA) models — all on Trossen Robotics’ accessible, real-world hardware, using the same infrastructure pioneered by the team at Physical Intelligence.


What is OpenPI and why does it matter?

OpenPI is an open-source robotics framework developed by Physical Intelligence. It supports large-scale training and evaluation of general-purpose robotic models like π₀ and π₀.₅ — both of which are open-source and available via the OpenPI GitHub repo.

These models represent a leap forward for embodied AI. They let robots follow language instructions, interpret visual scenes, and act across multiple robot embodiments, without task-specific retraining.

Key features include:

  • PaliGemma: A powerful vision-language encoder

  • Flow Matching: Smooth trajectory prediction

  • Action Chunking: Efficient, low-latency execution

Together, they form a flexible control system that makes zero-shot and few-shot learning possible — and now, you can run it on Trossen AI arms.


How does the OpenPI integration work?

Trossen Robotics has created a dedicated fork of the OpenPI repository that includes:

  • Support for the Trossen AI Stationary Kit

  • Training + inference workflows using π₀ and π₀.₅

  • Integration with Hugging Face for datasets and checkpoints


This allows you to:

  • Collect episodes using LeRobot

  • Train/fine-tune π₀/π₀.₅ models on real-world tasks

  • Run inference on your robot directly from the OpenPI client


Documentation for Trossen AI integration

We’ve prepared a complete integration guide that walks you through the entire process:

  • How to set up OpenPI for use with Trossen hardware

  • How to collect datasets using our AI arms

  • How to fine-tune and evaluate policies like π₀ and π₀.₅

  • Example configurations, hardware tips, and more

Whether you're training your first VLA model or deploying in production, this guide is the place to start.


What’s new in π₀.₅: from skills to semantics

π₀ demonstrated that generalist robotic control is possible across multiple platforms. π₀.₅ advances that idea by adding stronger semantic reasoning and a hierarchical architecture. Instead of simply learning physical actions, π₀.₅ is designed to generalize across new, unseen environments — making it more adaptable to real-world scenarios.

What makes π₀.₅ special is how it combines heterogeneous data sources: classical demonstrations, high-level semantic instructions, web-sourced imagery, and natural language. The goal is to build common-sense understanding on top of physical control skills.


*π₀.₅ Architecture (Courtesy: Physical Intelligence)*

At its core, π₀.₅ introduces a two-stage architecture:

  • First, a high-level planner predicts semantic goals (what needs to happen).

  • Then, a low-level action decoder — based on diffusion models trained via flow matching — generates continuous motor commands.

A key improvement is how π₀.₅ injects timestep information into the action decoder using a dedicated MLP module. This subtle change has been shown to improve performance, especially when synchronizing reasoning and movement.


Why does π₀.₅ matter?

These advancements help π₀.₅ bridge the gap between understanding *what* needs to be done and executing *how* to do it — a significant challenge in robotics. The model is better suited for out-of-lab environments, where variability, noise, and unexpected conditions are the norm.

More robust hierarchical reasoning, richer training data, and semantic grounding mean less task-specific fine-tuning and a step closer to general-purpose robotic agents.


Limitations to be aware of

Despite the progress, π₀.₅ still faces challenges:

  • Precision manipulation (such as folding laundry with exact folds or threading a needle) remains unreliable, because the system is purely vision-based and lacks tactile feedback.

  • Recovery from failure is limited. The model struggles to replan or recover from unexpected mistakes.

  • It still relies on high-quality sensors, powerful GPUs, and controlled environments. Operating in cluttered, dynamic spaces like real homes remains a challenge.


Early results

We ran π₀.₅ inference on our bimanual WidowX-AI arms, and the results were promising:

  • Successful pick-and-handover behavior with minimal tuning

  • Struggled with unfamiliar object shapes/colors (as expected)

  • Demonstrated smooth motion under camera-aligned control loops

It’s still early, and we’re refining the setup — but this validates our direction: generalist robot models running on real, accessible hardware.

*Inference Results (Fine-Tuned π₀.₅ for Block Transfer)*


What’s next

This is just the beginning. In the coming weeks, we’ll publish:

  • A full walkthrough video for training + deployment

  • Tools to help you adapt π₀/π₀.₅ to your own datasets

  • Benchmarks on policy generalization with Trossen AI arms

Whether you’re a researcher, developer, or robotics startup, OpenPI + Trossen AI is a stack you can build on. For more on our latest work, follow along with our robotics and VLA updates.


Stay tuned.


Tags:

  • Robotics

  • VLA

  • Machine Learning

  • Physical Intelligence

  • Artificial Intelligence


Unlocking New Possibilities?

  • Clone the dedicated OpenPI fork with Trossen AI Stationary Kit support to get started.

  • Collect episodes on Trossen AI arms using LeRobot for real-world tasks.

  • Fine-tune π₀ or π₀.₅ policies using the integrated training and inference workflows.


How the Integration Works??

  • Clone the dedicated OpenPI fork with Trossen AI Stationary Kit support to get started.

  • Collect episodes on Trossen AI arms using LeRobot for real-world tasks.

  • Fine-tune π₀ or π₀.₅ policies using the integrated training and inference workflows.

_Learn more about Trossen Robotics and Trossen SDK for your deployment._


Deployment readiness at a glance

_Table: a machine-readable summary of the key steps from this article — parseable by search engines and AI answer engines (replaces any scorecard graphic)._

#

Step

What it means

1

Clone the dedicated OpenPI fork with Trossen AI Stationary K

Clone the dedicated OpenPI fork with Trossen AI Stationary Kit support to get st

2

Collect episodes on Trossen AI arms using LeRobot for real

world tasks-

3

Fine

tune π₀ or π₀-₅ policies using the integrated training and inference workflows-

4

Connect Hugging Face for datasets and checkpoints

Connect Hugging Face for datasets and checkpoints

5

Run inference on your robot directly from the OpenPI client

Run inference on your robot directly from the OpenPI client

6

Follow the complete integration guide for setup, hardware ti

Follow the complete integration guide for setup, hardware tips, and example conf

π₀.₅ Architecture
π₀.₅ Architecture (Courtesy: Physical Intelligence)

Frequently Asked Questions

What is OpenPI?

OpenPI is an open-source robotics framework developed by Physical Intelligence. It supports large-scale training and evaluation of general-purpose robotic models like π₀ and π₀.₅, both available via the OpenPI GitHub repo.


How are Trossen AI arms integrated into OpenPI?

We created a dedicated fork of the OpenPI repository that adds support for the Trossen AI Stationary Kit, training and inference workflows using π₀ and π₀.₅, and Hugging Face integration for datasets and checkpoints.


What can I do with the integration?

You can collect episodes using LeRobot, train or fine-tune π₀/π₀.₅ models on real-world tasks, and run inference on your robot directly from the OpenPI client.


What is new in π₀.₅?

π₀.₅ adds stronger semantic reasoning and a hierarchical two-stage architecture: a high-level planner predicts semantic goals and a low-level action decoder generates continuous motor commands, helping it generalize to new, unseen environments.

Inference Results (Fine Tuned π₀.₅ for Block Transfer)

What are the limitations of π₀.₅?

Precision manipulation remains unreliable because the system is purely vision-based and lacks tactile feedback, recovery from failure is limited, and it still relies on high-quality sensors, powerful GPUs, and controlled environments.


What were the early results on Trossen hardware?

We ran π₀.₅ inference on our bimanual WidowX-AI arms and saw successful pick-and-handover behavior with minimal tuning and smooth motion under camera-aligned control loops, though it struggled with unfamiliar object shapes and colors.


What is coming next?

In the coming weeks we'll publish a full walkthrough video for training and deployment, tools to adapt π₀/π₀.₅ to your own datasets, and benchmarks on policy generalization with Trossen AI arms.

Comments

Rated 0 out of 5 stars.
No ratings yet

Add a rating

OUR PROMISE TO YOU

We stand behind our products with an industry-leading commitment to reliability, service,
and long-term support—because we believe performance should be measured in years, not months.

BUILT FOR REAL-WORLD RESEARCH ENVIRONMENTS. COVERS DEFECTS IN MATERIALS AND WORKMANSHIP. WEAR COMPONENTS ARE FIELD-REPLACEABLE AND READILY AVAILABLE.