top of page

Bimanual Robot Arm Systems: Evaluation Criteria for AI Research

Oct 8
11 min read

A bimanual robot arm can make coordinated two-hand tasks practical to study, but choosing a system is not just a matter of counting degrees of freedom or comparing arm specifications. Research teams need to understand how both arms move together, whether they can reach the task workspace, how they are calibrated and observed, and how the full setup fits the lab's software and data workflow. The right evaluation starts with the experiments and the evidence the team needs to produce.

What should a bimanual robot arm system enable?

Answer: It should support repeatable two-arm experiments with sufficient workspace, coordinated control, observable motion, and a data path suited to the research question.

A two-arm setup is useful when a task depends on complementary actions: one arm stabilizes an object while the other manipulates it, both arms act on separate objects, or the robot must coordinate a handoff. Before reviewing platforms, describe the experiment in terms of actions and constraints. That keeps the evaluation tied to the actual workflow instead of a feature checklist.

Write down a small set of representative tasks. Include the simplest task the system must perform, a typical experiment, and a demanding case that tests the limits of the setup. For each one, note:

  • Objects and contact:

    What is grasped, pushed, held, assembled, or transferred? Include the range of object sizes, shapes, and surface properties relevant to the work.

  • Coordination:

    Do both arms need to move at once, or does one hold a stable pose while the other acts? Are there handoffs or synchronized contact events?

  • Workspace:

    Where are the objects, fixtures, bins, and cameras? Which positions must be reachable by one arm, and which require coordinated access by both?

  • Observation:

    What must the team see or measure to judge success? Consider object pose, gripper state, arm pose, contact, and the task outcome.

  • Repeatability:

    How will the team reset the scene, record a trial, identify a failure, and run the next attempt under comparable conditions?

This task description should also identify what is outside the scope. For example, a laboratory may initially need a fixed workbench and a small set of tabletop tasks rather than mobile manipulation. A clear boundary makes it easier to compare a stationary setup with broader platform options without paying for capabilities that do not advance the current experiment.

Teams planning a broader platform evaluation can review the robotics hardware guide and the research platform overview as starting points. The key is to connect each candidate to a specific task, not to infer fit from a product label.

Start with the task geometry and operating envelope

Answer: Map the shared workspace first, then check each arm's reach, payload, mounting, and clearance against the objects and poses the experiment actually requires.

Reach is more than a maximum extension number. A robot may technically reach a point while being poorly positioned to approach it, maintain a stable grasp, or avoid the other arm. Sketch the work surface and the important task zones. Mark the start pose, grasp locations, handoff area, fixture positions, and any region that a camera or person must access.

For each task zone, ask whether one or both arms must reach it. Identify poses that require the arms to cross, pass close to each other, or work on opposite sides of an object. Those cases can reveal interference issues that are invisible in a single-arm reach estimate. Check the system's mounting height and orientation, work-surface dimensions, and the clearance needed for grippers and attached tools. Leave room for cable routing and camera placement instead of treating those as late additions.

Payload should be evaluated at the end effector, not as an isolated headline value. The gripper, adapter, sensor, and any tool attached to an arm contribute to the carried load. Also consider how the load changes through the task: a tool may be light, while a grasped object adds weight or shifts the center of mass. The relevant question is whether the system can execute the required motion with the intended configuration and acceptable repeatability.

Make a task envelope table before narrowing the options. Use measured dimensions when available; otherwise record estimates and flag them for confirmation. Treat the table as a working document, not as proof that the setup will succeed.

Evaluation item

Record for each task

Why it matters

Reach zones

Object positions, approach direction, and required poses

Shows whether each arm can reach useful configurations, not just a boundary point

Payload and tools

Object mass estimate, gripper, adapter, and sensor load

Captures the full working configuration

Shared workspace

Overlap, crossings, handoff positions, and clearance

Surfaces collision and coordination constraints

Mounting and access

Table height, arm spacing, service access, and camera positions

Connects the platform footprint to the practical lab arrangement

Trial outcome

Observable success conditions and repeatability needs

Turns platform evaluation into a measurable experiment

Compare the task envelope to candidate configurations only after recording these requirements. A stationary AI research platform or a bimanual workstation may suit fixed tabletop work, while other workflows may call for a different arrangement. The purpose of comparison is to identify what must be verified in a demonstration or integration test.

How should teams evaluate synchronization and calibration?

Answer: Verify that both arms can be commanded and observed against a shared timing and coordinate model, then test that relationship with repeatable calibration checks.

For coordinated manipulation, two independent arm interfaces are not automatically a coordinated system. The control architecture should make it clear how commands are issued to each arm, how state is read back, and how a task-level action relates to both arms. Ask how simultaneous motion is represented, how timing is handled, and what happens if one arm reaches a target earlier than the other.

Define the coordination requirement in plain terms. A task may need the arms to begin a motion together, maintain a relative pose, or perform a handoff in a particular sequence. These are different requirements. A shared interface can make a workflow easier to structure, but the team still needs to test latency, command timing, and state reporting in its own setup. Record the control rate and timing behavior that matter to the experiment rather than assuming the word synchronized guarantees a particular performance level.

Calibration connects the robot, work surface, cameras, and objects in a common frame. Start by listing the coordinate frames the application uses, such as the base of each arm, the tabletop, the camera, and the end effector. Document how each transform is established and how the lab will notice if it changes after equipment is moved. A calibration routine that works once but cannot be repeated after a camera adjustment is a fragile foundation for a data collection study.

Plan a simple verification routine. Move each arm to a small set of known locations, check the relationship between the two arms, and confirm that the camera's view aligns with the workspace reference. Repeat the checks after changing a tool, repositioning a camera, or moving a fixture. Keep the measurements and configuration notes alongside trial data so that a team can distinguish model behavior from setup drift.

Useful questions for a technical review include:

  • Can both arm states be read through the same application workflow?

  • Can the team issue coordinated commands without hiding the individual arm state?

  • How are coordinate frames named and configured, and can a researcher inspect them?

  • What calibration steps are documented, and how does the team repeat them?

  • Can failures and timing differences be logged in a way that supports debugging?

Robot performance evaluation has long treated measurable, comparable criteria as important to communication about robot systems; the NIST publication on performance evaluation of programmable robots provides background on that principle. For bimanual work, teams should define the measures that match their task rather than treating one generic score as a substitute for experimental validation.

Build the sensing and end-effector plan into the evaluation

Answer: Select cameras and end effectors as part of one task system, because visibility and contact behavior shape the data and the actions the robot can perform.

Camera placement should follow the experiment's observation needs. An overhead view can show the overall scene, while a wrist-mounted view can show local interaction; the exact arrangement depends on what the task requires. Check whether both arms, the object, and the contact area remain visible during critical actions. Occlusion is especially important when one arm blocks the other or covers the object at the moment the task changes state.

List the views and measurements needed to interpret a trial. Consider whether the work needs a fixed external camera, a camera attached to an arm, or more than one view. Then determine how images are associated with robot state and actions in the data record. Teams should consider mounting stiffness, field of view, lighting, cable routing, and whether camera movement will invalidate calibration. An attractive image is not enough if the relevant event is hidden or cannot be aligned with the robot's state.

End effectors deserve the same task-specific review. A gripper that is appropriate for one object may not support a different grasp, tool use, or contact behavior. For each task, document the grasp types, object range, required compliance or rigidity, and any tool changes. Include the end effector's mass and geometry in the reach and payload review, and check that its shape does not create unexpected interference when the arms work together.

Research groups should also evaluate how practical it is to swap, configure, and document tools. A modular approach can help teams explore alternatives, but only when adapters, mounting, software configuration, and calibration steps are understandable. Keep a configuration record for each experiment: tool identity, mounting arrangement, relevant settings, and any calibration change. That gives future users enough context to reproduce the setup.

For manipulation research that depends on learning from demonstrations, the system's data workflow matters as much as its camera hardware. Explore how a robotics data collection SDK and the available ALOHA research ecosystem relate to the team's intended capture and analysis process. The research literature on behavior-based control for assistive bimanual manipulation is one example of work that treats two-arm interaction as a coordinated manipulation problem, rather than merely placing two manipulators in one scene.

Evaluate ergonomics, software, and support as one workflow

Answer: A usable system gives researchers room to work, clear tools for operating and extending the setup, and a support path that helps resolve integration questions over time.

Ergonomics includes more than operator comfort. Consider how a researcher loads objects, resets a task, reaches emergency controls, changes end effectors, and accesses cables or connectors. A dense workstation can make a simple reset slow or obstruct camera views. If people will teleoperate the robot, assess the operator's posture and visibility during long sessions, the location of controls, and whether the interface keeps the task state understandable.

Think through the full cycle of a trial: set up the scene, initialize the system, run the task, inspect the outcome, save the record, and reset. Note which steps require a specialist and which can be handled by a student or colleague after onboarding. The goal is not just a successful first demonstration. It is an operating routine that different team members can follow consistently.

Software evaluation should cover the interfaces researchers will use and maintain. Confirm how the arms are configured, how commands are sent, how state is inspected, and how the setup connects to the team's ROS or machine-learning workflow where applicable. Look for developer-friendly documentation and examples that explain assumptions, dependencies, and common setup steps. Ask how the software is versioned and how a lab can reproduce an environment after a system update.

Open tooling can make it easier to inspect and adapt a workflow, but openness is only useful when the team can understand the components and maintain its changes. Map the boundary between hardware controls, robot drivers, data capture, and model or application code. That boundary helps the lab identify where a fault belongs and decide which parts need to be integrated with existing infrastructure.

Also ask how recorded data moves from a local experiment to storage, review, and model training. Teams with larger data programs may need a plan for dataset organization, permissions, and transfer to shared or cloud-connected infrastructure. The Trossen Cloud overview can inform that conversation, while the data collection solutions page is relevant for teams considering repeatable collection beyond a single lab workflow. Evaluate those options against the institution's actual security and infrastructure requirements; do not assume a service meets requirements that the institution has not reviewed.

Finally, make support part of the technical due diligence. Identify how the team can get help with setup, software questions, replacement parts, and troubleshooting. Check that support documentation matches the equipment and workflow under consideration. A clear support path and access to technical learning resources can help a team plan for ongoing operation, not just acquisition. For a specific platform comparison, review the relevant robot arm family and verify its fit against the task envelope directly.

Use a staged evaluation, not a feature-score shortcut

Answer: Move from task definition to configuration review, hands-on verification, and a documented acceptance plan so the team can expose unknowns before scaling the workflow.

A weighted scorecard can organize discussions, but it cannot replace testing. Start with must-have requirements such as workspace access, the coordination model, required tools, observation, and data capture. Separate those from preferences such as a particular mounting style or room for future expansion. If a candidate does not meet a must-have, a high score on unrelated features should not hide the gap.

  1. Define the experiment.

    Select representative tasks and write down measurable success conditions, operating constraints, and required data.

  2. Map the complete configuration.

    Include both arms, end effectors, cameras, mounting, work surface, cables, and software interfaces.

  3. Identify assumptions.

    Mark uncertain reach, timing, calibration, sensing, integration, and support details for confirmation.

  4. Run a focused verification.

    Test representative motions and interactions, including a case that exercises coordination and visibility rather than only free-space movement.

  5. Document acceptance criteria.

    Record what passed, what needs adjustment, and what must be true before the team expands collection or adds users.

Keep evidence close to the decision. For each requirement, record the test, result, configuration, and unresolved question. This makes it easier for a principal investigator, lab manager, engineering lead, or procurement team to understand both the value and the remaining integration work. It also supports a more useful follow-up discussion with a platform provider.

Frequently Asked Questions

Answer: Evaluate the complete coordinated setup against the intended experiments, and confirm the interfaces, workspace, sensing, and operating workflow through representative tests.

What is the first requirement to define for a bimanual robot arm?

Define the task and the two arms' roles. State what each arm must do, where objects and fixtures sit, what coordination is required, and how the team will determine whether a trial succeeded. Those details guide reach, payload, sensing, and software decisions.

Does a bimanual system need both arms to move at the same time?

Not every two-arm task requires simultaneous motion. Some require one arm to hold an object while the other acts; others require synchronized movement, a handoff, or coordinated contact. Specify the timing behavior the task needs, then test that behavior with the system's command and state interfaces.

How should a research team check whether the arms can reach its task?

Map the work surface, object positions, approach directions, and handoff or fixture zones. Check useful poses for each arm, shared workspace, tool clearance, mounting height, and camera access. Verify representative task configurations rather than relying only on a maximum reach figure.

Why include calibration and cameras when comparing arm hardware?

Calibration relates the arms, workspace, and cameras to one another. Camera placement determines whether important actions are visible and whether recorded observations can be interpreted alongside robot state. Both affect whether experiments can be repeated and analyzed.

What should a team request before selecting a platform?

Bring a task envelope, required end effectors and sensors, software expectations, data needs, and a list of unresolved assumptions. Ask for a configuration review and a way to verify critical requirements using representative tasks. Record what is confirmed and what still needs integration work.

Plan your bimanual robot arm evaluation

A strong evaluation connects the robot configuration to the research workflow from the first object interaction through calibration, data capture, analysis, and repeated trials. With the task requirements written down and the uncertain details made explicit, a team can choose a setup that supports its next experiment while leaving a clear path for future development.

 
 
 

Comments

Rated 0 out of 5 stars.
No ratings yet

Add a rating

OUR PROMISE TO YOU

We stand behind our products with an industry-leading commitment to reliability, service,
and long-term support—because we believe performance should be measured in years, not months.

BUILT FOR REAL-WORLD RESEARCH ENVIRONMENTS. COVERS DEFECTS IN MATERIALS AND WORKMANSHIP. WEAR COMPONENTS ARE FIELD-REPLACEABLE AND READILY AVAILABLE.
LIFETIME SUPPORT FOR TROSSEN PRODUCTS 

Follow Us On Social

  • LinkedIn
  • Youtube
  • Facebook
  • GitHub
  • Twitter
  • Instagram
  • TikTok

© 2026 Trossen Robotics. All Rights Reserved.

bottom of page