Embodied AI Hardware: Choosing the Physical Stack for Robot Learning
Choosing embodied AI hardware is not simply a matter of picking a robot arm. A useful research stack connects the manipulator and end effector to cameras, compute, controllers, a teleoperation interface, and, when the work requires it, a mobile base. The right combination lets a team repeat a task, inspect what happened, and build on the result rather than spending each experiment rebuilding the setup.
What belongs in an embodied AI hardware stack?
Answer: The core stack is a task-capable robot, an appropriate gripper, synchronized sensing, control and compute, and a human interface for setup or teleoperation. Add mobility only when the experiment includes movement through the environment.
Think of the system as a chain of connected decisions. The arm determines where and how the robot can reach. The gripper determines what contact and object interaction are possible. Cameras capture evidence of the scene and action. Controllers and compute translate commands into motion and support data capture or learning workflows. The operator interface makes it possible to collect demonstrations and monitor the robot.
A component can work well on its own and still be a poor fit for the full workflow. For example, a capable arm does not solve a data collection problem if the camera view misses the interaction or the control interface makes demonstrations inconsistent. For physical AI work, integration and repeatability matter as much as a component's headline specification.
Research teams can use a system such as a Solo AI platform or a Stationary AI platform as a point of comparison when scoping single-arm and stationary bimanual work. The goal is not to select a platform by name first. It is to map the experiment requirements to hardware roles and confirm that those parts operate together.
How should you choose manipulators and grippers?
Answer: Start with the motion and contact demands of the task, then select an arm and gripper that cover those demands with enough repeatability and room for the planned experiments.
Write down the actions a successful episode requires: reaching a target, approaching an object, grasping it, moving it, releasing it, or using a tool. Note the workspace, the range of object sizes and shapes, and whether the robot needs one arm or coordinated bimanual motion. This is more actionable than beginning with a long list of degrees of freedom or payload figures without a task context.
For the manipulator, check reach and usable workspace first. A nominal reach figure does not tell you whether the arm can approach an object from the direction your experiment needs, avoid nearby fixtures, or reach the entire work surface. Also consider payload as a system constraint: the end effector, cables, and grasped object all contribute to what the arm must handle. Review the mounting arrangement and the space required around the robot for cameras, objects, and operator access.
Then match the gripper to the contact strategy. Parallel-jaw grippers can suit many pick-and-place studies involving objects that provide accessible opposing surfaces. Other tasks may need a different hand geometry or a specialized tool. Consider the object variation in the dataset, how grasp success will be observed, and how quickly an operator can reset the scene. If a study relies on one narrow object set, the simplest suitable gripper may be sufficient. If it spans varied objects and interactions, the end effector can become a major experimental variable.
For a single-arm research setup, compare the available WidowX robot arms and WidowX AI manipulator options against reach, mounting, tooling, and workflow needs. For two-arm manipulation, examine the ALOHA kits and Workbench bimanual station in light of the tasks and teleoperation approach. These links are starting points for evaluating configurations, not a substitute for checking the technical requirements of a specific experiment.
Test the arm in the same physical arrangement you expect to use for data collection. A bench edge, camera stand, cable bundle, or operator position can limit motion even when the arm's nominal workspace appears adequate. Mark the usable work area and run the complete approach, grasp, transfer, and release sequence at representative locations. Check whether the robot can return to a consistent start pose and whether objects or fixtures need precise placement to make the task repeatable.
Plan for maintenance and iteration as well as the first demonstration. Identify which parts of the setup are likely to change as the research question develops: the gripper, object fixture, camera mount, or arm arrangement. Prefer a layout that provides access to those components without requiring the whole cell to be rebuilt. Keep a record of the tool, mount, and relevant robot configuration used for each dataset so that changes in hardware are visible during analysis.
Which cameras and sensing components matter?
Answer: Select camera placement and sensing based on what the dataset or control loop must observe, and verify that the views remain useful throughout the robot's motion.
Begin with the observations needed to interpret an episode. A scene camera can show the work area and object context. A wrist-mounted view can expose details near the end effector. A team may use one or both perspectives, depending on whether the task depends on broad scene context, close contact, or both. Before adding cameras, sketch their fields of view and inspect likely occlusions from the arm, gripper, operator, and fixtures.
Ask practical questions: Can the camera see the object before and after contact? Does the robot block the grasp? Can the view distinguish a successful placement from an attempted one? Are the images captured at a rate and resolution useful for the intended analysis? Can camera frames be associated with actions and other sensor records on a shared timeline? A multi-view rig is only helpful when its views add useful information and can be managed consistently.
Lighting and background are part of the sensing setup. Changing reflections, shadows, or object placement can alter what a camera records. Document camera mounts, positions, and relevant scene conditions so that a later session can be reconstructed. If the study intentionally varies these conditions, record the variation rather than allowing it to drift unnoticed.
For a data-focused workflow, consider how capture and export will fit together. Trossen's data collection SDK page describes the software side of the workflow; hardware planning should ensure that the intended observations and robot actions can be captured consistently. A camera specification alone does not guarantee synchronized, training-ready episodes.
Include calibration and synchronization in the commissioning plan. Record camera positions and any calibration procedures used, and establish how image timestamps relate to robot state and commands. Check sample episodes for missing frames, unexpected delays, and view changes when the arm reaches the edges of its workspace. If a sensor is repositioned, treat that as a meaningful configuration change and repeat the relevant checks instead of assuming the existing recordings remain directly comparable.
Consider what a later reviewer will need to interpret a sample. The camera should make task success or failure distinguishable, and the episode should retain enough context to understand the object and starting conditions. A tightly cropped view can make contact easier to inspect but remove scene context; a broad view can establish context while hiding small interactions. A planned combination of views can balance those needs, provided the views can be handled consistently across sessions.
Compute and control hardware for robot learning
Answer: Size compute for the work that will run locally, and treat motor control, data capture, and learning workloads as related but distinct requirements.
A robot control process needs predictable communication with actuators and sensors. A training or simulation workload may require substantial CPU, memory, storage, or GPU resources. Those jobs may share a machine or use separate systems, but the decision should be based on measured workload and the control architecture, not on a general assumption that one powerful workstation solves every requirement.
List the tasks expected of the compute setup: robot control, camera acquisition, visualization, logging, simulation, data preprocessing, or model training. Establish which of them must run during physical trials and which can happen afterward. Check the interfaces and software support needed by the selected robot and sensors, then estimate storage from the expected session length, sensor streams, and number of repetitions. Leave practical headroom for debugging and new workloads, while avoiding a specification built around an untested future requirement.
Keep actuator control and high-level policy execution conceptually clear. A policy can issue actions, while a lower-level controller handles device-specific motion behavior. Define how commands move between those layers, what happens when communication is interrupted, and how an operator can stop or reset an experiment. This boundary makes it easier to diagnose whether an issue came from perception, policy output, control, or hardware.
A workstation such as the TOTL workstation may be relevant when a project needs dedicated local compute, but match it to the actual mix of development and data workloads. Teams building toward shared storage or remote training can also review Trossen Cloud as part of infrastructure planning. Decide where data lives, who can access it, and how it moves from collection to analysis before sessions produce large volumes of files.
Make compute selection testable. Run the robot, capture sensors, and save a representative episode with the applications and visualization tools the team expects to use. Observe whether the system remains responsive and whether recordings complete as intended. Repeat with the anticipated number of cameras and a realistic session duration. This provides a more useful basis for sizing than a peak performance figure alone.
Storage planning should include a repeatable naming and backup practice. Decide how to identify a run, where its raw data and derived files belong, and how to verify that an episode copied successfully. Separate original captures from processed versions so that a preprocessing change does not erase the record of what the robot initially observed. Teams should also consider access permissions and retention expectations before collection begins.
Keep an interface inventory for the full system. Record the connections required by arms, cameras, operator devices, and compute, along with any hubs or adapters needed in the planned layout. Confirm that cables can be routed without obstructing motion or creating trip hazards, and leave access for service. Small interface and layout omissions can consume setup time even when every major component has been selected correctly.
Add a mobile base when the task requires it
Answer: Add a mobile base when the research question includes navigation or manipulation from changing locations; keep the initial system stationary when mobility does not contribute to the experiment.
A mobile manipulator combines movement through the environment with arm interaction. This can support tasks where the robot must approach multiple work areas or collect data across locations. It also introduces new variables: base positioning, movement repeatability, changes in camera viewpoint, and coordination between the base and arm. Those variables affect experiment design, setup, and interpretation of results.
Before choosing a base, define the environment and routes the robot must use. Consider floors, thresholds, available turning space, charging or operating plans, and how the arm will be secured during movement. Specify whether the base must stop at a known pose before manipulation or act while moving. Decide how the data will record base motion and the arm's actions together. If the experiment does not need mobile behavior, a stationary workstation can make it easier to isolate manipulation variables.
For teams exploring mobile manipulation, the Rivet mobile manipulation robot and Mobile AI platform pages provide relevant hardware references. Compare them to the work area, manipulation tasks, and required data rather than treating mobility as an automatic upgrade.
For a first study, isolate base and arm behavior in stages. Establish a repeatable route or set of stopping locations, then test whether the base reaches those locations consistently enough for the manipulation task. Next, check arm access at each stop and verify that the cameras retain useful views. If both base movement and arm manipulation vary at once, it can be difficult to determine which part of the system explains a changed outcome.
Define safety and operational boundaries for the intended environment before running autonomous or teleoperated trials. Identify the permitted operating area, how a person can pause or stop the system, and how the robot is returned to a known state after an interrupted run. Document those procedures alongside the task protocol. This is especially useful when tests involve multiple operators or move beyond a single fixed workstation.
Interfaces for repeatable experiments
Answer: The operator interface should let a trained person command, observe, pause, and reset the robot in a consistent way while preserving the data needed to understand each episode.
Teleoperation is often central to collecting demonstrations. Evaluate whether the interface maps naturally to the desired movement, whether the operator can see relevant camera views, and whether the robot responds in a controllable way. For bimanual demonstrations, consider whether one operator can manage both arms and whether the interface supports the coordination required by the task. Practice with representative objects before collecting a large dataset; awkward controls can introduce inconsistent demonstrations and operator fatigue.
Also define the experiment protocol around the interface. Establish how each episode starts and ends, how the scene is reset, what counts as completion, and what to do after a failed grasp or unexpected motion. If different operators collect data, document the same instructions for everyone. Record useful identifiers such as task version, object condition, operator, and session, subject to the team's data practices. A structured protocol helps separate real task variation from changes in how the study was run.
Dedicated teleoperation equipment, such as the Glide and Cockpit interface, should be assessed in the context of operator workflow and robot configuration. For handheld data collection, review TRumi as a distinct approach. The useful question is which interface makes the desired interaction and data capture repeatable for your team.
Embodied AI research also depends on connecting physical action to data structures and software tools. Review the Interbotix robotics software information and the broader Trossen AI platform overview alongside hardware requirements. When teams describe embodied AI as systems that perceive and act through physical bodies, the physical stack is what makes that interaction observable and testable; see the research overview Embodied AI: From LLMs to World Models. A separate review frames trustworthy physical AI as a path from theory toward practice, reinforcing the value of deliberate system-level validation: Towards Trustworthy Physical AI: From Theory to Practice.
A hardware comparison before purchase
Answer: Compare complete workflows against the experiment, not isolated component specifications. Use the same task, sensing, data, and operator criteria for every candidate system.
The table below is a scoping aid. It does not rank products. Use it to identify tradeoffs and the information your team still needs to confirm for its specific application.
Hardware element | What it enables | Questions to resolve | Common tradeoff |
Manipulator | Reach, positioning, and object interaction | Does the workspace cover the task? What payload and mounting arrangement are needed? | More capability may add setup and integration demands |
Gripper or end effector | Contact with objects and tools | What surfaces, shapes, and grasp types must the task handle? | A specialized tool can help a defined task but narrow flexibility |
Cameras | Scene and interaction observations | Which views are needed? Are occlusion and synchronization manageable? | More views add data and calibration work |
Compute and controller | Robot control, data acquisition, and local workloads | Which jobs run during trials? What interfaces and storage are required? | Consolidation can simplify equipment but complicate workload isolation |
Mobile base | Movement between work locations | Does the study require navigation? Can base position be repeated? | Mobility expands task scope and introduces additional variables |
Operator interface | Teleoperation, monitoring, and episode control | Can users perform and reset the task consistently? | Specialized interfaces may improve a workflow but require training |
For each candidate, rate whether it supports the core task, whether the team can run it with available space and staff, how easily it can be extended, and what must be validated before a study begins. Then make a short end-to-end test plan: assemble the setup, run a representative task, capture a complete episode, inspect the data, and repeat the task under the same protocol. That trial often reveals gaps that a component-by-component review misses.
Teams looking for a broader system view can use the hardware guide and academic research solutions as additional starting points. For work centered on larger-scale collection, see the robotics data collection overview. Confirm current technical details directly against the configuration under consideration.
Before making a final selection, separate requirements into must-haves, useful options, and future possibilities. Must-haves are conditions that determine whether the planned experiment can run at all, such as reach to the work area or visibility of the critical interaction. Useful options reduce repeated setup effort or support additional variations. Future possibilities should not be allowed to obscure the immediate validation plan. This distinction helps teams discuss platform tradeoffs clearly across researchers, lab managers, and technical buyers.
Finally, agree on a small acceptance test before the system arrives or is commissioned. Specify a representative task, the number of repeat runs, which data records should exist, and what an operator must be able to do to pause and reset. The test need not prove that a learned policy will succeed. It should establish that the physical and data collection workflow is ready to support the research question, and make open integration questions visible early.
Frequently Asked Questions
Answer: The best starting point is a defined task and a complete, testable hardware workflow, rather than the largest possible component list.
Do I need a mobile robot for embodied AI research?
No. A mobile base is useful when movement through an environment is part of the task. A stationary setup can be a better starting point for isolating manipulation, teleoperation, or data capture variables.
Should cameras be mounted on the robot or around the workspace?
It depends on what the experiment needs to observe. A fixed scene camera can provide workspace context, while a wrist view can show the interaction near the gripper. Test likely occlusions and confirm that the selected views can be synchronized with action data.
Can one compute system handle control and model training?
It may be possible, but the decision depends on the robot interfaces, control timing, and compute demands of the workloads. Identify which processes must run during trials, then test them together before relying on a shared machine in a study.
What should a team test before collecting a large dataset?
Run representative episodes from start to finish. Check robot motion, camera visibility, operator control, reset steps, and the completeness and timing of saved data. Repeat the same task to see whether the setup and protocol produce consistent records.
Build around the experiment, then validate the stack
Embodied AI hardware works best as a coordinated research system: a manipulator and suitable end effector, sensing that captures relevant events, control and compute matched to the workload, and an interface that supports repeatable operation. Add a mobile base when the question requires mobility, and verify the complete data path with a representative experiment before scaling collection. For a wider view of embodied systems, a recent review discusses physical AI from theory toward practice at this research review. A deliberate, task-first selection process gives teams a more reliable foundation for learning from physical interaction.